Just Encase
  • Challenges & Projects
  • Design Challenges
  • Just Encase
  • More
  • Cancel
Just Encase
Blog [Pool Water Monitoring] #6 Kit first steps
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Just Encase to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: feiticeir0
  • Date Created: 21 Dec 2021 7:08 PM Date Created
  • Views 1051 views
  • Likes 9 likes
  • Comments 2 comments
  • adafruit's DS18B20
  • DS18B20 Hight Temperature probe
  • lora
  • justencase
  • Arduino MKR WAN 13000
  • just_encase
  • just encase
Related
Recommended

[Pool Water Monitoring] #6 Kit first steps

feiticeir0
feiticeir0
21 Dec 2021

image

Hi everyone. Hope you're all safe.

KIT

Yesterday the kit finally arrived (thank you Element14) and it's awesome.

image

Start testing

Today, was time to test some of the components. This was my first experience with an Arduino MKR 1300 WAN.  I haven't yet tried the IoT Cloud or LoRa, but that time will come.

So, I've decided to test Adafruit's High Temperature Probe DS18B20.

image

According to Adafruit's learning tutorials, for this probe, the colors are has follows (The tutorial is for CircuitPython, but the wiring colors are the same):

Probe Wiring Arduino
Solid White GND
White with Orange Stripe VCC or 5V
White with Blue Stripe SIGNAL

For the Arduino MKR 1300 WAN, VCC outputs 3.3V through the on-board voltage regulator. This voltage is 3.3V if USB or VIN is used and equal to the series of the two batteries when they are used. The 5V pin outputs 5V from the the board when powered from the USB connector or from the VIN pin of the board. It is unregulated and the voltage is taken directly from the inputs.

Code

The code was taken directly from Arduino website.

#include <OneWire.h>
#include <DallasTemperature.h>

#define ONE_WIRE_BUS 3

OneWire oneWire(ONE_WIRE_BUS);

DallasTemperature sensors(&oneWire);

float Celcius=0;
float Fahrenheit=0;
void setup(void) {
  
  Serial.begin(9600);
  sensors.begin();
}

void loop(void) { 
  sensors.requestTemperatures(); 
  Celcius=sensors.getTempCByIndex(0);
  Fahrenheit=sensors.toFahrenheit(Celcius);
  Serial.print(" C  ");
  Serial.print(Celcius);
  Serial.print(" F  ");
  Serial.println(Fahrenheit);
  delay(1000);
}

After powering the Arduino, here's the result

image

Next Friday will try Lora communication with both Arduinos, transmitting some temperature values.

Merry Christmas

  • Sign in to reply
  • feiticeir0
    feiticeir0 over 4 years ago in reply to christophesky

    Thank you christophesky

    Merry Christmas !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • christophesky
    christophesky over 4 years ago

    Great write up :) Merry Christmas!