Products
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
Make Life Accessible
  • Challenges & Projects
  • Design Challenges
  • Make Life Accessible
  • More
  • Cancel
Make Life Accessible
Blog Make Life Accessible - Motor Suite Test - blog 8
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 29 May 2016 9:24 PM Date Created
  • Views 2495 views
  • Likes 7 likes
  • Comments 19 comments
  • make life accessible
  • pmsm_motor_control
  • accessibility_projects
  • kinetis_motor_suite
  • mla
  • clear_walk
Related
Recommended

Make Life Accessible - Motor Suite Test - blog 8

dougw
dougw
29 May 2016

This entry is a first exploration of the Kinetis Motor Suite capabilities, demonstrating motor reversing and sequencing through several states.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Next time I will try to hook up the Hall effect sensors to see if I can work at lower speeds.

 

Relevant Links

MLA Design Challenge

 

The full set of Clear Walk project blogs can be found here:

Make Life Accessible

  • Sign in to reply

Top Comments

  • kulky64
    kulky64 over 10 years ago +2
    How do you think will Hall effect sensors help you at lower speeds? The state of the Hall effect sensors changes every 60 degrees of electrical revolution. This is of little help to FOC algorithm. They…
  • shabaz
    shabaz over 10 years ago in reply to dougw +2
    Hi Doug, The hall sensors should always allow you to know which phase in the commutation cycle you're at (i.e. even with a stall), whereas with the sensorless method you won't know at very slow speeds…
  • kulky64
    kulky64 over 10 years ago in reply to dougw +2
    All true, but applies to BLDC motor with six-step commutation (sometimes called block commutation). But you are dealing with PMSM motor and Field Oriented Control (FOC) with all three phases driven at…
  • dougw
    dougw over 10 years ago in reply to DAB

    Hi DAB.

    I have not looked at the TI approach.

    I noticed when setting a low speed demand that the system would eventually lose its correct commutation timing, especially under load, and just vibrate back and forth. It still seems to have enough torque to rotate, (after all, I am running with no load) - it just seems the commutation timing is no longer correct. I guess if it is not spinning, there is no back-emf to sense commutation position.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 10 years ago in reply to kulky64

    The way I understand it, BLDC motors require sensing to know when to commutate the phases. When the speed is high enough, there is enough back-emf in the un-powered phases to deduce rotor position and figure out commutation timing. When rotation is not fast enough for significant back-emf or perhaps when no computer is available, Hall sensors can be used instead. NXP has an application note that might help explain it better:

    http://www.nxp.com/files/microcontrollers/doc/app_note/AN4058.pdf

    I don't know if it will work better, since I have never done anything tricky with a BLDC motor, but I seem to recall reading somewhere that hooking up the Hall effect sensors would provide better low speed control.

    Doug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Nice update Douglas.

     

    I am curious about your low speed issues.  Is it a case of needing the right sequence and is that an issue for how you can load the motor?

     

    Have you looked at the similarities with the TI Instaspin approach?

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kulky64
    kulky64 over 10 years ago

    How do you think will Hall effect sensors help you at lower speeds? The state of the Hall effect sensors changes every 60 degrees of electrical revolution. This is of little help to FOC algorithm. They may help you if you are using trapezoidal control as back-EMF zero crossing detection is not reliable at low speeds, but FOC algorithm will probably use some other means of sensorless rotor position estimation.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<