Products
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
Make Life Accessible
  • Challenges & Projects
  • Design Challenges
  • Make Life Accessible
  • More
  • Cancel
Make Life Accessible
Blog Step Three:  3.2 Programming environment based on KDS3.2.0+SDK1.3.0
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fyaocn
  • Date Created: 28 Jun 2016 7:28 AM Date Created
  • Views 1111 views
  • Likes 1 like
  • Comments 3 comments
  • accessibility_projects
Related
Recommended

Step Three:  3.2 Programming environment based on KDS3.2.0+SDK1.3.0

fyaocn
fyaocn
28 Jun 2016

1. As I have mentioned in last blog. The KMS1.0.0.0 seems do not work well. With different mixed type installation for drivers, IDE and SDK. Finally, my development environment has come to good result and work OK now. PMSM-demo has passed the debug and report no more errors.

image

2. Tips to share.

2.1 The reasons that Kinetic Motor Suit (KMS) can not control linix Motor is that,

img firmware in the  FRDM-KV31FFRDM-KV31F board is incompatible with the version of KMS New.out file shall be flashed into the memory of KV31F

- Driver shall be properly installed, in order that UART port can be found.

- The path of SDK shall be correctly defined, since SDK1.3.0 shall be needed for KMS to work well.

2.2 The demo project comes with the KMS can not  pass build stage. Since some of the files in the project can not be found in present developing environment. While there is not enough time for me to check one by one. So I have to skip this demo project.

2.3 The demo-project in Quick Start Guide can pass the debug, while the function of motor control is not tested yet.

2.4 With preliminary study, I assumed that the incompatibility comes with Real Time OS. For Freescale, MQX is first choice in SDK 1.3.0. But following upgrade seems slow and FreeRTOS become first choice in SDK 2.0. I can not prove the assumption now. So, I use SDK1.3.0 in my programming.

2.5 When using KSD3.2.0, Run-Debug configuration shall be defined first and New Lauch Group shall be added and properly selected or the KDS will return with error code (1) instaed.

 

3. Suggestion

It would be safe to use old stable version IDE,  SDK,  and even Demo-project. If new function has some alternative choice, try older version instead before one can master all the technical detail.

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 10 years ago in reply to fyaocn +1
    Never mind, keep on progressing. Personal goals more important. Clem
Parents
  • fyaocn
    fyaocn over 10 years ago

    Unfortunately it is, but I have just figured out what to do and tried to complete the project by deadline. That is what challenge really means.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to fyaocn

    Never mind, keep on progressing. Personal goals more important.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 10 years ago in reply to fyaocn

    Never mind, keep on progressing. Personal goals more important.

    Clem