Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog ERROR: Task (/tools/petalinux-v2019.1-final/components/yocto/source/aarch64/layers/meta-browser/recipes-browser/chromium/chromium_54.0.2810.2.bb:do_compile) failed with exit code '1'
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
  • Author Author: buffteethr
  • Date Created: 2 Dec 2019 9:35 PM Date Created
  • Views 1037 views
  • Likes 2 likes
  • Comments 3 comments
Related
Recommended

ERROR: Task (/tools/petalinux-v2019.1-final/components/yocto/source/aarch64/layers/meta-browser/recipes-browser/chromium/chromium_54.0.2810.2.bb:do_compile) failed with exit code '1'

buffteethr
buffteethr
2 Dec 2019

Hi,

Has anyone gotten these Errors when trying to build ?

 

| collect2: fatal error: ld terminated with signal 9 [Killed]

| compilation terminated.

| ninja: build stopped: subcommand failed.

| WARNING: /home/buffteethr/petalinux/2018_3/support_documents/v2/lab2/lab2_example/build/tmp/work/aarch64-xilinx-linux/chromium/54.0.2810.2-r0/temp/run.do_compile.20276:1 exit 1 from 'ninja -v -j 2 chrome chrome_sandbox chromedriver'

| ERROR: Function failed: do_compile (log file is located at /home/buffteethr/petalinux/2018_3/support_documents/v2/lab2/lab2_example/build/tmp/work/aarch64-xilinx-linux/chromium/54.0.2810.2-r0/temp/log.do_compile.20276)

ERROR: Task (/tools/petalinux-v2019.1-final/components/yocto/source/aarch64/layers/meta-browser/recipes-browser/chromium/chromium_54.0.2810.2.bb:do_compile) failed with exit code '1'

NOTE: Tasks Summary: Attempted 9909 tasks of which 2085 didn't need to be rerun and 2 failed.

 

 

Summary: 2 tasks failed:

  /tools/petalinux-v2019.1-final/components/yocto/source/aarch64/layers/meta-xilinx-tools/recipes-bsp/pmu-firmware/pmu-firmware_git.bb:do_patch

  /tools/petalinux-v2019.1-final/components/yocto/source/aarch64/layers/meta-browser/recipes-browser/chromium/chromium_54.0.2810.2.bb:do_compile

Summary: There were 3 WARNING messages shown.

Summary: There were 3 ERROR messages shown, returning a non-zero exit code.

ERROR: Failed to build project

 

Thanks,

Cary

  • Sign in to reply
  • buffteethr
    buffteethr over 6 years ago in reply to rscasny

    No problem. I am actually enjoying the PIIP. I really really like the Xilinx tools and devices now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 6 years ago

    Cary,

     

    Thanks for all the blogs! Quite a number of them.

     

    Randall

    --element14 team

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nerdyupdates
    nerdyupdates over 6 years ago

    Yes, I definitely had the Chromium issue. I think I commented it out or added a command to exclude that from the build in one of the make files somewhere, as I couldn't find where it was included in the PetaLinux build tools. Who wants a bloated browser in an embedded Linux build anyway? I had another issue with webkitgtk which I didn't have the patience to resolve. My hope for the project is to just utilize one of the pre-existing PetaLinux builds and then install kernel modules / applications after the fact as needed.