Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog Finally Installed Vivado, Xilinx SDK, and PetaLinux but versions 2019.1
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
  • Author Author: buffteethr
  • Date Created: 15 Oct 2019 3:58 PM Date Created
  • Views 2068 views
  • Likes 5 likes
  • Comments 4 comments
Related
Recommended

Finally Installed Vivado, Xilinx SDK, and PetaLinux but versions 2019.1

buffteethr
buffteethr
15 Oct 2019

I installed the Vivado and Xilinx SDK tools along with Petalinux using the instructions from the link: http://avnet.me/AvnetTTC_VM  [OracleRegistered VM VirtualBox Installation Instructions for Windows and Linux Virtual Machine Creation Targeting Avnet Development Boards]

They use versions of the tools from 2018. However, I installed the 2019.1 version of everything including Petalinux. I modified a few things unique to me. It was mostly error free however I ran into an issue with the Petalinux install.

 

I used gksudo gedit /etc/xinetd.d/tftp to Create /etc/xinetd.d/tftp.

 

I find it easier to use gedit for editing in Ubuntu than vi or nano.

 

I ran into a weird permission issue with running ./petalinux-v2019.1-final-installer.run

 

I had to do a chmod 777 on the file to finally get it to work.

 

The final result are shown below:

image

 

 

 

image

image

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +2
    I found the different versions of Vivado were a real pain - especially IP,s sample code or guides that wouldn't work with a newer version and weren't updated.
  • aspork42
    aspork42 over 7 years ago +1
    I just found in HW Lab 4, there is a TCL script that we have to run, and it checks for the version of Vivado, and requires it to match 2018.3. You could probably just change the script manually to look…
Parents
  • Fred27
    Fred27 over 7 years ago

    I found the different versions of Vivado were a real pain - especially IP,s sample code or guides that wouldn't work with a newer version and weren't updated.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 7 years ago

    I found the different versions of Vivado were a real pain - especially IP,s sample code or guides that wouldn't work with a newer version and weren't updated.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • cmelement14
    cmelement14 over 7 years ago in reply to Fred27

    I concur based on my experience. Hopefully 2019 version doesn't give Cary any headache ahead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aspork42
    aspork42 over 7 years ago in reply to Fred27

    I agree as well. It could make trouble shooting harder since you won’t know if there is a compatibility issue or something else. Good luck with the training!