Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog PYNQ+Ultra96-V2 and Wifi???
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
  • Author Author: buffteethr
  • Date Created: 22 Dec 2019 5:07 AM Date Created
  • Views 2286 views
  • Likes 2 likes
  • Comments 3 comments
Related
Recommended

PYNQ+Ultra96-V2 and Wifi???

buffteethr
buffteethr
22 Dec 2019

Has anyone here run into an issue with the PYNQ v2.5 image for the Ultra96-V2 and WIfi? The wlan0 does not show up with the ifconfig command. I did some digging and noticed that there is NO wpa_supplicant.conf file is missing.

  • Sign in to reply

Top Comments

  • cmelement14
    cmelement14 over 6 years ago +2
    You don't need to configure Wifi through shell. Instead, configure it through python environment. The following is what I did and it works perfect. xilinx@pynq:~$ sudo python3 [sudo] password for xilinx…
  • buffteethr
    buffteethr over 6 years ago in reply to cmelement14 +1
    Thanks that worked. My Wifi is up and running. Now I cant ping out. Weird. It is not and issue as I have my usb WEBCAM project running but I may need to update somethings using the internet.
Parents
  • cmelement14
    cmelement14 over 6 years ago

    You don't need to configure Wifi through shell. Instead, configure it through python environment. The following is what I did and it works perfect.

     

    xilinx@pynq:~$ sudo python3

    [sudo] password for xilinx:

    Python 3.6.5 (default, Apr  1 2018, 05:46:30)

    [GCC 7.3.0] on linux

    Type "help", "copyright", "credits" or "license" for more information.

    >>> from pynq.lib import Wifi

    >>> port = Wifi()

    >>> port.connect("your_wifi_essid","your_wifi_password")

    ifdown: interface wlan0 not configured

    Internet Systems Consortium DHCP Client 4.3.5

    Copyright 2004-2016 Internet Systems Consortium.

    All rights reserved.

    For info, please visit https://www.isc.org/software/dhcp/

    Listening on LPF/wlan0/f8:f0:05:c3:30:96

    Sending on   LPF/wlan0/f8:f0:05:c3:30:96

    Sending on   Socket/fallback

    DHCPDISCOVER on wlan0 to 255.255.255.255 port 67 interval 3 (xid=0x7928c939)

    DHCPDISCOVER on wlan0 to 255.255.255.255 port 67 interval 3 (xid=0x7928c939)

    DHCPDISCOVER on wlan0 to 255.255.255.255 port 67 interval 5 (xid=0x7928c939)

    DHCPREQUEST of 192.168.1.214 on wlan0 to 255.255.255.255 port 67 (xid=0x39c92879)

    DHCPOFFER of 192.168.1.214 from 192.168.1.1

    DHCPACK of 192.168.1.214 from 192.168.1.1

    bound to 192.168.1.214 -- renewal in 21017 seconds.

    >>>

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • buffteethr
    buffteethr over 6 years ago in reply to cmelement14

    Thanks that worked. My Wifi is up and running. Now I cant ping out. Weird. It is not and issue as I have my usb WEBCAM project running but I may need to update somethings using the internet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • buffteethr
    buffteethr over 6 years ago in reply to cmelement14

    Thanks that worked. My Wifi is up and running. Now I cant ping out. Weird. It is not and issue as I have my usb WEBCAM project running but I may need to update somethings using the internet.