Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Blog Blog 1 : Getting Started with the Hardware
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: thareeq
  • Date Created: 27 Jul 2023 5:51 PM Date Created
  • Views 549 views
  • Likes 4 likes
  • Comments 0 comments
Related
Recommended

Blog 1 : Getting Started with the Hardware

thareeq
thareeq
27 Jul 2023

The Hardware Includes : 

  1. Ultra96-v2 MPSoC board with SD card
  2. USB to JTAG/UARTPOD
  3. 96 Boards Click starter Kit
  4. Power Adapters

image

Ultra96-v2 specification : 

  • Xilinx Zynq UltraScale+ MPSoC ZU3EG A484
  • Micron 2 GB (512M x32) LPDDR4 Memory
  • Microchip Wi-Fi / Bluetooth
  • Mini DisplayPort (MiniDP or mDP)
  • 1x USB 3.0 Type Micro-B upstream port
  • 2x USB 3.0, 1x USB 2.0 Type A downstream ports
  • 40-pin 96Boards Low-speed expansion header
  • 60-pin 96Boards High-speed expansion header
  • 85mm x 54mm form factor
  • Linaro 96Boards Consumer Edition compatible
  • 12 V power input
  • power button and reset button
  • 4 User LEDs
  • MicroSD card socket
  • 1 user Push button

The Hardware comes with a small getting started note (lets follow that): 

1. Go to avnet.me/ultra96-v2-oob to download the boot image

2. Use BalenaEtcher to flash the image to SD card

3. Insert SD card in ultra96-v2. Set the Boot mode switch (SW3) to SD boot as shown in the image (by default it is in SD boot)

4.Power ON and press and release the power button (SW4)

5. Once done the Blue Done LED will illuminate.

6. You can connect to ultra96's hotspot and go to 192.168.2.1 to be greeted with ultra96v2 home page

imageimageimage