Path to Programmable 3

Table of contents ...  

design challenge profile

element14 and AMD invite all members to enroll in Path to Programmable III; a free training program that includes an FPGA-based SoC giveaway and a design/build phase where selected participants will have the opportunity to win up to $4000 in prizes.

Learn, Create, and Design with FPGA-based SoCs


What is Path to Programmable III?

Path III is the third session in the element14 Community’s structured FPGA-based SoC training. The first Path was held in 2018 and focused on programmable logic devices PLDs and featured the AVNET MiniZed development board, based on the AMD Zynq™ 7000 SoC.

Path II convened in 2019 and offered more advanced learning opportunities and featured the AVNET Ultra96-V2 development board, based on the AMD Zynq™ UltraScale+ MPSoC.

Path III will double the fun by offering structured trainings on both the MiniZed (2021.1) and Ultra96-V2 (2021.2) boards. Each training track will be followed by a design/build phase. To spice up the competition, we are offering up to $4000 in prizes and four different design paths.

What is a Design Path?

Every Path to Programmable training has a learning phase and a design/build phase. After participants complete the training modules (2021.1 & 2021.2) and receive a development board, they will design and build a project following one of four design paths:

The Vision Path

  • Embedded/Machine Vision
  • Face Recognition
  • Accelerated AI Video
  • Image/Video Streaming

The Core Technology Path

  • AI/Machine Learning
  • Connectivity
  • DSP
  • Ethernet

The Market Path

  • Health
  • Home
  • Gaming
  • Industrial

The Environmental Path

  • Dirt & Plants
  • Streets & Highways
  • Pets & Critters
  • Water & Oceans

The Kit

We are offering two different development kits that members can choose between on their application form. 

The 2 Sponsored Boards
kit
 Buy Now   Tech Specs

MiniZed - (50 available kits)

The MiniZed training will teach you to develop a Zynq™ 7000 platform using AMD Software and Hardware tools within an Ubuntu OS running in a virtual machine, while learning the Zynq 7000 architecture. The training includes three modules: Software, Hardware, and PetaLinux.

Training 2021
kit
 Buy Now   Tech Specs

Ultra96-V2 - (20 available kits)

The Ultra96-V2 training training will teach you how to get started with the AMD Zynq™ MPSoC. This series of three training modules will walk you through the three main elements of the design process: hardware design within VivadoTm, Embedded Software Design in VitisTm and Embedded Linux development using Petalinux.

Training 2021

The Prizes

Prize Prize Category

Grand Prize Winner

Grand Prize

Approximate Value $1900 USD*

  • MP720025 US Digital Oscilloscope
  • HP OMEN 17-ck1020nr 17.3" Gaming Laptop Computer

Runner Up

Runner Up

Approximate Value $1000 USD*

MP720644 US CAL DU Oscilloscope

Third Prize

Third prize

Approximate Value $600 USD*

FLIR C3-X WIFI Thermal Imager

Fourth Prize

Finisher prize

Approximate Value $400 USD*

FLUKE-175 ESFP Handheld Digital Multimeter

Honorable Mentions

Finisher prize

Approximate Value $134 USD*

  • DIGILENT 410-376 Dev Board
  • MP730651 Handheld Digital Multimeter

Finisher Prize** swag: t-shirts or any of the element14 branded items we already have. Pins, pens, shirts, etc.

*Or local equivalent
**Grand, Runner-Up, 3rd Prize, 4th Prize Winners, and Honorable Mentions will not receive a finisher prize.

The Dates

Project Phases Dates
Application Period 31st March 2023
Application Deadline 14th May 2023
Participants Announced 17th May 2023
Training Begins 26th May 2023
Training Ends 26th July 2023
Training Blogs for Credit Due 27th July 2023
Build Period 28th July - 28th August 2023
Final Project Blog Due 5th September 2023
Winners Announced September 2023
Prizes Shipped September 2023

Eligibility

Any element14 member is eligible to enroll. If you are not a Community member please register here to join.

Application Tips

An important thing to remember is that you are also competing against others to become a participant in this program. Therefore, everything starts with the application.

The key to writing a winning application is to provide as much meaningful information about yourself as possible. Try answering each of the following questions in your application:

  1. Describe your technical background.
  2. Why are you interested in this training program?
  3. What development board do you prefer: the MiniZed or the Ultra96-V2
  4. What design path are you most interested in and why?
  5. Have you participated in the element14 Community? If so, please provide some links to what you have done (forum posts, blogs, reviews, etc.). If you are a new member, answer "New Member."

All interested element14 members must submit an application entry form before the end of enrollment. See the The Dates above.

Technical Resources

Go here for the course documentation.

The Judges

element14 Community Staff
image
Top Member(s)
image

Awarding Points: We will award up to 40 points per training blog for up to 5 training blogs only. If you write a tutorial or how you solved a problem, you will earn more points than if you wrote a general update blog such as “I received the board” blog. The final project blog is worth up to 300 points, as determined by our judges. All training blogs and projects must be published in the Path to Programmable 3 group by the due date, see the deadline table.

The Challengers

You will be able to see how you compare to other participants via a tracking table here (Updated: Sept 27, 2023 by rscasny):

Blog 1
40 pts
Blog 2
40 pts
Blog 3
40 pts
Blog 4
40 pts
Blog 5
40 pts
Final Project
300 points
Total Points
500
abhishek2018: Ultra96-V2 -1
40 40 40 40 40 230 430
adrian.cad: Ultra96-V2 -2
0 0 0 0 0 0 0
alrms: Ultra96-V2 -3
0 0 0 0 0 0 0
cghaba: Ultra96-V2 -4
40 40 40 40 0 125 285
daxlar: Ultra96-V2 -6
0 0 0 0 0 0 0
fyaocn: Ultra96-V2 -7
40 40 40 40 40 153 353
jovarela: Ultra96-V2 -8
40 0 0 0 0 0 40
lfb: Ultra96-V2 -9
30 0 0 0 0 0 30
manihatn: Ultra96-V2 -10
40 40 40 40 40 250 450
manojroy123: Ultra96-V2 -11
40 40 40 40 0 0 160
pandoramc: Ultra96-V2-12
40 40 40 40 40 183 383
poponianhua: Ultra96-V2 -13
0 0 0 0 0 0 0
prashanthgn.engineer: Ultra96-V2 -14
40 40 40 40 40 205 405
pratyush_cetb: Ultra96-V2 -15
0 0 0 0 0 0 0
rahulkhanna: Ultra96-V2 -16
40 0 0 0 0 0 40
rajivbishwokarma: Ultra96-V2 -17
40 40 40 40 40 255 455
saadtiwana_int: Ultra96-V2 -18
40 40 40 40 40 260 460
thareeq: Ultra96-V2 -19
40 40 0 0 0 0 80
vinayyn: Ultra96-V2 -20
30 0 0 0 0 0 30
Adnan.: MiniZed-2 -21
0 0 0 0 0 0 0
anushyab: MiniZed -22
40 40 40 40 40 0 200
asraf7: MiniZed -23
0 0 0 0 0 0 0
Bub1st: MiniZed -24
0 0 0 0 0 0 0
ciorga: MiniZed -25
40 40 40 40 40 240 440
flyingbean: MiniZed -26
40 40 40 40 40 210 410
Gennadiy: MiniZed -27
0 0 0 0 0 0 0
guillengap: MiniZed -28
40 40 40 40 40 225 425
gurustaad: MiniZed -29
0 0 0 0 0 0 0
hal2069rw: MiniZed -30
0 0 0 0 0 0 0
javagoza: MiniZed -31
40 40 40 40 40 270 470
jd2020: MiniZed -32
0 0 0 0 0 0 0
Kingdom: MiniZed -33
0 0 0 0 0 0 0
MarioDL99: MiniZed -34
0 0 0 0 0 0 0
navadeepganeshu: MiniZed -35
40 40 40 40 40 215 415
pallen19: MiniZed -36
0 0 0 0 0 0 0
paulcastor30: MiniZed-2-37
0 0 0 0 0 0 0
RDuran: MiniZed -38
0 0 0 0 0 0 0
Riya_101: MiniZed -39
0 0 0 0 0 0 0
shmulikl: MiniZed -40
0 0 0 0 0 0 0
sndpvrmah: MiniZed -41
0 0 0 0 0 0 0
svnagendra2003: MiniZed-2 -42
0 0 0 0 0 0 0
taifur: MiniZed -43
40 40 40 40 40 208 408
vishnu123: MiniZed -44
30 30 0 0 0 0 60
Yalugem: MiniZed -45
0 0 0 0 0 0 0

Where to Ask Questions?

For any general or technical questions about the competition, please post a comment on this page. It is monitored by element14.

Bookmarking this page is a good way to keep up-to-date with the competition.

The Terms

Please read the full terms and conditions attached below.

Anonymous
Parents
  • Just to be clear that this "challenge" means a successful applicant will have to follow and report on the training course and then apply that knowledge to a real life project that fits in one of the design paths outlined above.

    Is that correct?

    I'm asking because I believe the application must mention that final real life project and if that's the case, I need to think a bit more about it than just "play with it to light a led when it recognizes my phone by bluetooth"

  • Yes, you gpo through the traning modules and then build a project, which will be judges by our judges. I don't think getting an LED to flash will get you the grand prize!

Comment Children
No Data