Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Forum Connect to webserver error
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 129 subscribers
  • Views 823 views
  • Users 0 members are here
  • ultra96
  • Path Programmable III
Related

Connect to webserver error

luciaom_02
luciaom_02 over 3 years ago

Hello, I’m using a ultra96-V2 board and I’m trying to set up the wifi connection, following the guide and I’m running into some problems.
I’m reading chapter 8, “Connect to Webserver”, but I can’t set up the network called Ultra96-V2_<MAC_ADDRESS>. When I run ./wifi.sh, I get an error with the configuration of the LAN:

root@ultra96v2-2020-1:~# ./wifi.sh
Stopping Connection Manager
ifdown: interface wlan0 not configured
Successfully initialized wpa_supplicant
[ 85.017404] power up request for already powered up source Wifi
[ 85.023330] Device already up. request source is Wifi
[ 85.028409] wilc_sdio mmc1:0001:1 wlan0: Failed to get mac address
[ 85.034600] wilc_sdio mmc1:0001:1: wilc_sdio_disable_interrupt
Could not set interface wlan0 flags (UP): Invalid argument
nl80211: Could not set interface 'wlan0' UP
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
wlan0: Failed to initialize driver interface

When I run this file step by step, I get an error when I run ifdown and I get the following output:

ifdown: interface wlan0 not configured

I have tried using ip link set wlan0 down instead and that seems to work and doesn’t report any error. 

Then if I keep running the wifi.sh script, one command at a time, it raises an error when reaching ifup.
When I run either ifup wlan0 or ip link set wlan0 up, I get the following error:

[ 883.500230] power up request for already powered up source Wifi
[ 883.506161] Device already up. Request source is Wifi
[ 883.511239] wilc_sdio mmc1:0001:1 wlan0: Failed to get mac address
[ 883.517421] wilc_sdio mmc1:0001:1: wilc_sdio_disable_interrupt
RTNETLINK answers: Invalid argument


Perhaps, is the ploblem in the wifi/bluethoot module? Is there any step that I‘m skipping? Could there be a file incompatibility problem?

Has anyone had the same problem?

  • Sign in to reply
  • Cancel
Parents
  • javagoza
    0 javagoza over 3 years ago

    I don't have the ultra96-V2 but the MiniZed. This is what I get when running wifi.sh on the MiniZed:

    root@minized-sbc-base-2021-1:~# wifi.sh
    Copy the wpa_supplicant.conf file from eMMC to /etc.
    NOTE!  This file must have been previously edited with
    the WLAN SSID and password!
    Mount the eMMC.
    mount: /mnt: special device /dev/mmcblk1p1 does not exist.
    Copy the wpa_supplicant.conf file from eMMC to /etc.
    Unmount the eMMC.
    umount: /mnt: not mounted.
    Bringup the WiFi interface.
    Successfully initialized wpa_supplicant
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    rfkill: Cannot open RFKILL control device
    Fetch an IP address from the DHCP server.
    udhcpc: started, v1.32.0
    udhcpc: sending discover
    udhcpc: sending discover
    udhcpc: sending select for 192.168.1.37
    udhcpc: lease of 192.168.1.37 obtained, lease time 43200
    /etc/udhcpc.d/50default: Adding DNS 80.58.61.250
    /etc/udhcpc.d/50default: Adding DNS 80.58.61.254
    root@minized-sbc-base-2021-1:~#

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • javagoza
    0 javagoza over 3 years ago

    I don't have the ultra96-V2 but the MiniZed. This is what I get when running wifi.sh on the MiniZed:

    root@minized-sbc-base-2021-1:~# wifi.sh
    Copy the wpa_supplicant.conf file from eMMC to /etc.
    NOTE!  This file must have been previously edited with
    the WLAN SSID and password!
    Mount the eMMC.
    mount: /mnt: special device /dev/mmcblk1p1 does not exist.
    Copy the wpa_supplicant.conf file from eMMC to /etc.
    Unmount the eMMC.
    umount: /mnt: not mounted.
    Bringup the WiFi interface.
    Successfully initialized wpa_supplicant
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    nl80211: kernel reports: Match already configured
    rfkill: Cannot open RFKILL control device
    Fetch an IP address from the DHCP server.
    udhcpc: started, v1.32.0
    udhcpc: sending discover
    udhcpc: sending discover
    udhcpc: sending select for 192.168.1.37
    udhcpc: lease of 192.168.1.37 obtained, lease time 43200
    /etc/udhcpc.d/50default: Adding DNS 80.58.61.250
    /etc/udhcpc.d/50default: Adding DNS 80.58.61.254
    root@minized-sbc-base-2021-1:~#