Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Week 3: Thermal Imaging Test of MiniZed FPGA
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
  • Author Author: snidhi
  • Date Created: 28 Oct 2018 11:38 AM Date Created
  • Views 1760 views
  • Likes 6 likes
  • Comments 6 comments
  • minized architecture
  • avnet minized
  • minized_content
Related
Recommended

Week 3: Thermal Imaging Test of MiniZed FPGA

snidhi
snidhi
28 Oct 2018

Out of curiosity, I decided this weekend to spend some time to measure the heat distribution on the Minized FPGA board and compare it to another fpga board. For this measurement I used the FLIR ThermoVision A20M 60Hz 160 x 120 Infrared Thermal Imaging Camera IR Imager. It was a fun experiment to do. Datasheet of the ThermoVision A20M

 

  • Introduction to ThermoVision A20M
  • The Test Setup
  • The Results of the Thermal Imaging Test
  • Conclusion

 

Introduction to ThermoVision A20M

 

The ThermoVision A20M is an accurate, intelligent infrared imaging and temperature measurement camera for industrial process monitoring, product verification, and security applications. It is used in the industry for precise temperature measurement and can output the video in real time using the FireWire or Ethernet connection.

 

image

 

image

The Specs of the FLIR ThermoVision A20M IR Imager Camera

 

The Test Setup

 

Here I measure the thermal profile of the MiniZED and the ARTY Z7 FPGA boards after the boards are programmed and turned ON. The test setup was done according to the manual of the FLIR ThermoVision A20M IR Imager.

 

image

 

image

An example test setup

 

image

image

Front side of the fpga boards

 

image

Back side of the boards

 

image

The GUI

 

The Results of the Thermal Imaging Test

 

The thermal measurement results are as below.

 

image

Fig: The color scale for all the below measurements

 

The Thermal Imaging of the Arty Z7 FPGA board

image

Front Side of Arty Z7 FPGA board

 


image

The Back side Arty Z7 FPGA board

 

image

The live measurement

 

 

The Thermal Imaging of the MiniZED FPGA board

image

Front Side of MiniZED FPGA board

 

image

Front Side of MiniZED FPGA board

 

 

A quick comparison between the MiniZED and the ARTY Z7 fpga boards in terms of where the maximum of the heat is localized.

 

image

Comparing the Front side of the fpga boards

 

image

Comparing the back side of the fpga boards

 

Conclusion

As seen from the pictures above; the bottom and the topside the Minized fpga board have a more uniform power consumption around the fpga area. It can be due to presence of more active power

components on the Minized board as compared to the Arty Z7. In the Arty Z7 board; most of the heat is concentrated on the fpga chip itself.

Such measurements can be helpful when designing the overall casing for these fpga boards. As one can clearly see which ares of the board need better thermal heatsink and to think about the proper heat dissipation of the housing/casing.

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +2
    That's a very nice thermal camera setup you have there. Interesting to see that the power management IC on the MiniZed is getting a little warm too. Other than that, it's all happening in the SoC but I…
  • aspork42
    aspork42 over 7 years ago +1
    Nice analysis. I was curious about the temperature and was thinking of doing a similar thing - I don't have to now My board does get quite warm which is what made me wonder about it. It would be interesting…
  • snidhi
    snidhi over 7 years ago in reply to aspork42 +1
    yes, I also did it for fun and out of curiosity. The power consumption definitely increases as the the fpga get more full with code and peripherals. I have seen this behavior in a previous project where…
  • snidhi
    snidhi over 7 years ago in reply to DAB

    I added the color scale separately now

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago

    Nice analysis.

     

    Do you have the color scale so we can see what the temperatures were?

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 7 years ago in reply to Fred27

    Thanks David, it was nice weekend fun

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago

    That's a very nice thermal camera setup you have there. Interesting to see that the power management IC on the MiniZed is getting a little warm too. Other than that, it's all happening in the SoC but I suppose that's not too surprising.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 7 years ago in reply to aspork42

    yes, I also did it for fun and out of curiosity.

    The power consumption definitely increases as the the fpga get more full with code and peripherals. I have seen this behavior in a previous project where I saw the current consumption rise upto 1.5Amps @12V after the fpga was fully programmed. 

    I think if you look into the power analysis window in the Vivado GUI it should give a approx idea for your project as of where the thermal and heat consumption is headed to

     

    Cheers

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>