Pi-Fest
  • Challenges & Projects
  • Design Challenges
  • Pi-Fest
  • More
  • Cancel
Pi-Fest
Blog Audio Encryption Project Blog 4: Encryption and Decryption
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: juno
  • Date Created: 10 Aug 2022 5:32 AM Date Created
  • Views 1225 views
  • Likes 6 likes
  • Comments 0 comments
  • Pi-Fest Design Challenge
  • raspberry pi pico
  • audio encryption
Related
Recommended

Audio Encryption Project Blog 4: Encryption and Decryption

juno
juno
10 Aug 2022

Tiny Jambu Encryption and Decryption

The Tiny Jambu algorithm is a lightweight cryptographic algorithm written in C by Hongjun Wu and Tao Huang and is available here. We started by testing the encryption and decryption functions from the Tiny Jambu library. Examples were provided to verify that encryption and decryption were working correctly. Although these functions have many arguments such as associated data, nonce, and secret message numbers, we mainly made use of plaintext, ciphertext, and the key and set the other variables to some default values. The plaintext, ciphertext, and key are stored using character arrays which we initialize using hex values for each character.

image

Figure: Example provided to test the code

One issue we had was finding an unused variable “nsec”. The variable is an argument to both the encryption and decryption functions but is not used at all, which confused us. Keeping it uninitialized seemed to work, however. Our guess is that since the Tiny Jambu library we used is the opt implementation they did not include the use of “nsec”. Below is one of the provided examples to test the code as well as our code providing the correct output.

int main(void){
    // variables
    const unsigned char m[] = {0x00};                                                   // plaintext
    unsigned long long mlen = sizeof(m);                                                // plaintext length
    const unsigned char c[] = {0xA1, 0x75, 0xD5, 0xB5, 0xC1, 0xEE, 0x4A, 0x0F, 0xA1};   // ciphertext
    unsigned long long clen = sizeof(c);                                                // ciphertext length pointer
    const unsigned char k[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F}; // 128-bit key

    encrypt(m, mlen, k);
    decrypt(c, clen, k);
    return 0;
}

Figure: Main function for testing encryption/decryption

void encrypt(const unsigned char* m, unsigned long long mlen, const unsigned char* k){
    unsigned long long c_length = 80;                               // ciphertext length
    unsigned char c[c_length];                                      // ciphertext
    unsigned long long *clen = &c_length;                           // ciphertext length pointer
    const unsigned char ad[] = {0x00};                              // associated data
    unsigned long long adlen = sizeof(ad);                          // associated data length
    const unsigned char *nsec;                                      // secret message number
    const unsigned char npub[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B};  // public message number

    crypto_aead_encrypt(c, clen, m, mlen, ad, adlen, nsec, npub, k);

    printf("\n");
    printf("Ciphertext = ");
    for (int i = 0; i < c_length; i++){
        printf("%02X", c[i]);
    }
    printf("\n");
}

Figure: Function to test encryption

void decrypt(const unsigned char* c, unsigned long long clen, const unsigned char* k){
    unsigned long long m_length = 80;                               // plaintext length
    unsigned char m[m_length];                                      // plaintext
    unsigned long long *mlen = &m_length;                           // plaintext length pointer
    const unsigned char ad[] = {0x00};                              // associated data
    unsigned long long adlen = sizeof(ad);                          // associated data length
    unsigned char *nsec;                                            // secret message number
    const unsigned char npub[] = {0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B};  // public message number

    crypto_aead_decrypt(m, mlen, nsec, c, clen, ad, adlen, npub, k);

    // print
    printf("Plaintext = ");
    for (int i = 0; i < m_length; i++){
        printf("%02X", m[i]);
    }
    printf("\n");
}

Figure: Function to test decryption

image

Figure: Correct encryption and decryption outputs

X3DH Key Exchange

The X3DH Key Agreement protocol was developed by Moxie Marlinspike and Trevor Perrin and is used by the Signal messaging app. The protocol has three phases: 

  1. Alice publishes her pre-keys (IKA and SPKA)  to a server
  2. Bob fetches a “pre-key bundle” from the server, verifies it, and sends an initial message to Alice
  3. Alice receives, verifies, and processes Bob’s initial message

We used an ED25519 library for all of our key generations. We edited the functions to only generate keys and not encrypt messages since we are using our own algorithm for that. We decided to use ED25519 instead of ED448 since the NSA has backdoor access to ED448. For the key derivation function required by X3DH we used HKDF. We used RFC6234 for verification of the keys. The output of our code is shown down below and shows that Bob and Alice both generate the same secret key.

image

Figure: X3DH steps

    //Generating long-term Identity Key pair for Bob
    ed25519_create_seed(bob_seed); //create randome seed
    ed25519_create_keypair(bob_id_public_key, bob_id_private_key, bob_seed); //create keypair out of seed 

    //Generate SignedPreKey Pair for bob
    ed25519_create_seed(bob_seed); //create random seed 
    ed25519_create_keypair(bob_spk_public_key, bob_spk_private_key, bob_seed); //create keypair out of seed

    ed25519_sign(bob_spk_signature, bob_id_public_key, bob_id_private_key);
    
    if (ed25519_verify(bob_spk_signature, bob_id_public_key)) {
        printf("\nvalid signature\n");
    } else {
        printf("\ninvalid signature\n");
        // Abort();
    }
    //Verifying on Alice's side
    ed25519_create_seed(alice_seed);
    ed25519_create_keypair(alice_id_public_key, alice_id_private_key, alice_seed);

    //Generate Ephemeral keys
    ed25519_create_seed(alice_seed);
    ed25519_create_keypair(alice_ephemeral_public_key, alice_ephemeral_private_key, alice_seed);

Figure: Generating keys

    if(hkdf(whichSha,salt,salt_len,dh_final,ikm_len,info,info_len,okm_integer,okm_len) == 0)
    {
        printf("HKDF is valid\n");
    } else {
        fprintf(stderr, "\nHKDF is invalid\n");
    }

    for(int i=0; i<okm_len;i++)
    {
        output_key[i] = okm_integer[i];
        // printf("%d\n", output_key[i]);
    }

Figure: Key derivation

image

Figure: X3DH key exchange verified