Pi-Fest
  • Challenges & Projects
  • Design Challenges
  • Pi-Fest
  • More
  • Cancel
Pi-Fest
Documents Pi-Fest Design Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 10 Mar 2022 2:15 PM Date Created
  • Last Updated Last Updated: 24 May 2022 3:12 PM
  • Views 15809 views
  • Likes 12 likes
  • Comments 30 comments
Related
Recommended

Pi-Fest Design Challenge

Make some noise with the Raspberry Pi Pico in the Pi-Fest music technology Design Challenge.

design challenge profile
Pi-Fest Design Challenge
About this Challenge | Dates | The Judges | The Kit | The Prizes | Example Application | Terms & Conditions | The Challengers

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The Challenge

Make some noise with the Raspberry Pi Pico!

This new musical Design Challenge will put you and the Raspberry Pi Pico center stage.

50 successful applicants will get a Raspberry Pi Pico free of charge to use to build and blog their project. For the chance to win one of the prizes below, you must blog your build process and the final outcome of your Raspberry Pi Pico music or audio project. Use the Raspberry Pi Pico and any other Raspberry Pi products of your choice to create your music or audio project.

Successful projects will feature on our Pi-Fest livestream and challengers will be featured on our Pi-Fest tour poster.

Example applications could include:

• Synthesizer
• Podcasting Rig
• Live Music Production Machine
• AI Music Machine
• Sound level logging and Monitoring

The Sponsored Kit The Specs
Raspberry Pi Pico - 50 will be given away
image
Buy Now

Raspberry Pi Pico

  • Raspberry Pi designed RP2040 chipset
  • Dual core ARM Cortex M0+ processor at up to 133MHz with variable core frequency
  • 264kB SRAM & 2MB onboard flash memory
  • 26 Multifunction GPIO pins (23x digital only, 3x ADC capable)
  • 2x SPI, 2x I2C, 2x UART, 3x 12-bit ADC and 16x controllable PWM channels

 

The Prizes

Prize Prize Category

Winning Headliner

Live Music and Podcasting Bundle

image

Approximate Value $950 USD*

  • $500 of Ticketmaster Vouchers
  • Shure SM7B Professional Microphone and Stand
  • Go XLR professional USB Audio Interface
  • Headline Position on our Livestreamed Festival
  • Headline Position on your very own Pi-Fest Tour Poster

Supporting Act

image

Approximate Value $550 USD*

  • $250 of Ticketmaster Vouchers
  • Shure MV7 USB Microphone
  • Headline Position on our Livestreamed Festival
  • Headline Position in your very own Pi-Fest Tour Poster
       

Finisher Prize**

image

To be a finisher you must complete 5 blogs and show us testing the resilience of their project.

Approximate Value $30 USD*

  • Multicomp Pro Multimeter

*Or local equivalent

**Grand Prize and Runner Up winners also earn the finisher prize.

 

The Judges

   

element14 Community Judges
element14 Community Team
image

 

The Dates

Project Phases Dates
Application Period 14th March 2022
Application Deadline 1st May 2022
Challengers Announced 8th May 2022
Build Period 8th May 2022 - 14th July 2022
Projects Due 14th July 2022
Winners Announced July 2022
Prizes Shipped July 2022

 


The Terms

 

Selected official applicants will be chosen to receive the "Kit" listed above; these successful applicants will be our sponsored challengers. The sponsored challengers must use the Raspberry Pi Pico within their project, and publish their final code and designs on the Community for others to use. Those not chosen as sponsored challengers may also join the competition and be eligible to win prizes, but they must base their projects around the Raspberry Pi Pico and adhere to all terms and conditions of the challenge.

Applicants must post their progress and final project as at least 5 blog posts before the closing date (see above), when projects are due. Challengers are strongly encouraged to post their blogs regularly during the contest period, rather than posting them all close to the finish of the competition.

Projects that use the Raspberry Pi Pico most creatively, along with posts that are media rich with photos, videos, and code samples will be viewed more favorably in the judging process.

Please read the full terms and conditions of the challenge, attached below.

 

Ready to join the challenge? Then apply here!

 

If you are not successful in becoming a sponsored challenger, but still want to enter, all you need to do is use the Raspberry Pi Pico as described above in your project and adhere to the same Terms and Conditions for a chance to be our winner! Non-sponsored challengers are eligible for the Finisher and Winner Prizes, as well.

  • design challenge
  • raspberry pi
  • pi-fest
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • skruglewicz
    skruglewicz over 4 years ago +2
    I heard about this challenge on LinkedIn, Surprising since I'm an active member of the Element14 community. I have participated in many design challenges and Roadtest here on Element14. I am a retired…
  • scottiebabe
    scottiebabe over 4 years ago +2
    If only I had musical talent LOL This sounds like yet another fun activity happening on E14. When the time comes I think I will tinker away at making pico wah effects pedal. I believe a wah pedal is…
  • feiticeir0
    feiticeir0 over 4 years ago in reply to mr_lindowsmac +2
    Usually they are announced on the page. They are late.
Parents
  • phoenixcomm
    phoenixcomm over 4 years ago

    I still need a usb text to Morse code for aircraft FAA station Id's. It will have a audio output which is sent to my radio Radio

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to phoenixcomm

    In the ham world (I'm not a ham, I have no qualifications), the "standard" seems to be Winkey (AKA Winkeyer), and an example implementation is WKUSB. It's not an open hardware project as far as I'm aware, but it could be possible to make one with the same interface I guess, so that any existing software could talk to it too, since the API is published (I believe). Anyway, maybe that's overkill, since perhaps just a Pi Pico (or Arduino etc) could be programmed to either key, or generate tones based on COM port input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 4 years ago in reply to phoenixcomm

    In the ham world (I'm not a ham, I have no qualifications), the "standard" seems to be Winkey (AKA Winkeyer), and an example implementation is WKUSB. It's not an open hardware project as far as I'm aware, but it could be possible to make one with the same interface I guess, so that any existing software could talk to it too, since the API is published (I believe). Anyway, maybe that's overkill, since perhaps just a Pi Pico (or Arduino etc) could be programmed to either key, or generate tones based on COM port input.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 4 years ago in reply to shabaz

    (can't edit).

    Looks like the ready-made chip was reasonable cost, $9.75 (still requires a USB-UART adapter though), but out of stock (from hamcrafters2.com website):

    image

    Diagrams from the PDF datasheet [no hyperlink button]: ( hamcrafters2.com/.../WK3_Datasheet_v1.3.pdf ), in case it's useful for a future open source/open hardware version:

    There are keyed outputs as well as audio output (sidetone pin). And fancy stuff like being able to adjust speed independently of the host computer.