• Products and Partners
    Products and Partners
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
Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] - Smarter Spaces #3 - Remote Horse Feeder System
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
  • Author Author: jomoenginer
  • Date Created: 9 Jul 2016 5:07 PM Date Created
  • Views 1248 views
  • Likes 2 likes
  • Comments 9 comments
Related
Recommended

[Pi IoT] - Smarter Spaces #3 - Remote Horse Feeder System

jomoenginer
jomoenginer
9 Jul 2016

So, I was able to get the iLumi controlled via a python script that in turn I was able to add to OpenHAB and could control the iLumi BR30 from an OpenHAB ColorPicker, however when I attempted to add the EnOcean Pi 902 to the Raspberry Pi 3 and performed the update/upgrade to support the device I lost both the Wi-Fi and the Bluetooth functionality of the Raspberry Pi 3.   I was able to recover the W-Fi connection on the RasPi 3 by performing a dist-upgrade and then updating the firmware on the system to 4.4.3.  This corrected the Wi-Fi issue but I am still unable to get the Bluetooth device on the RasPi 3 to enable.  The system seems to think there is no bluetooth device on the board which I know there is one since it was working prior to the upbreak.  I'll have to see if I can get this to come up again or just add a usb bluetooth dongle to the board to get past it.

This assisted me in getting the WiFi back up and working:

http://raspberrypi.stackexchange.com/questions/43474/how-to-enable-wi-fi-channel-12-on-raspberry-pi-3

 

Also, I was never able to get the RasPi to see the EnOcean Pi 902 so I was wondering if anyone knew if the device is supported with Raspberry Pi 3 and Jessie or do I need to use the RasPi B+ to connect the EnOcean Pi 902.  

  • Sign in to reply

Top Comments

  • fvan
    fvan over 10 years ago +2
    Hi Jon, i got my EnOceanPi 868 to work, including Wifi and BLE. All is described here: [Pi IoT] Alarm Clock #05: EnOcean Pi and Sensors Good luck! Frederick
  • jomoenginer
    jomoenginer over 10 years ago +1
    Still no success with getting the BLE device to enable, but I did find some more info regarding this. Apparently at kernel 4.4.9 there was a switch from ttyAMA0 to serial1; I'm currently running with 4…
  • jomoenginer
    jomoenginer over 10 years ago in reply to jomoenginer +1
    Okay, finally a bit of success. After searching the web and attempting many changes to the RasPi 3 config, I finally stumbled on the needed info to get the On Board BLE device working again on the RasPi…
Parents
  • jomoenginer
    jomoenginer over 10 years ago

    Still no success with getting the BLE device to enable, but I did find some more info regarding this.  Apparently at kernel 4.4.9 there was a switch from ttyAMA0 to serial1; I'm currently running with 4.4.14-v7+. I've gone through a few iterations of updates and reinstall of packages and reverted the settings back to use the UART for the BLE device but the device still will not enable. 

     

    This is what I see from  hciuart.service status

     

    pi@raspberrypi:~ $ sudo systemctl -l status hciuart.service

    ● hciuart.service - Configure Bluetooth Modems connected by UART

       Loaded: loaded (/lib/systemd/system/hciuart.service; enabled)

       Active: failed (Result: exit-code) since Sun 2016-07-10 11:45:36 PDT; 35s ago

      Process: 524 ExecStart=/usr/bin/hciattach /dev/serial1 bcm43xx 921600 noflow - (code=exited, status=1/FAILURE)

     

    Jul 10 11:45:36 raspberrypi hciattach[524]: Failed to reset chip, invalid HCI event

    Jul 10 11:45:36 raspberrypi hciattach[524]: Can't initialize device: Success

    Jul 10 11:45:36 raspberrypi hciattach[524]: bcm43xx_init

    Jul 10 11:45:36 raspberrypi hciattach[524]: Flash firmware /lib/firmware/BCM43430A1.hcd

    Jul 10 11:45:36 raspberrypi systemd[1]: hciuart.service: control process exited, code=exited status=1

    Jul 10 11:45:36 raspberrypi systemd[1]: Failed to start Configure Bluetooth Modems connected by UART.

    Jul 10 11:45:36 raspberrypi systemd[1]: Unit hciuart.service entered failed state.

     

    This is the link I am following:

    https://www.raspberrypi.org/forums/viewtopic.php?f=28&t=148305

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jomoenginer
    jomoenginer over 10 years ago

    Still no success with getting the BLE device to enable, but I did find some more info regarding this.  Apparently at kernel 4.4.9 there was a switch from ttyAMA0 to serial1; I'm currently running with 4.4.14-v7+. I've gone through a few iterations of updates and reinstall of packages and reverted the settings back to use the UART for the BLE device but the device still will not enable. 

     

    This is what I see from  hciuart.service status

     

    pi@raspberrypi:~ $ sudo systemctl -l status hciuart.service

    ● hciuart.service - Configure Bluetooth Modems connected by UART

       Loaded: loaded (/lib/systemd/system/hciuart.service; enabled)

       Active: failed (Result: exit-code) since Sun 2016-07-10 11:45:36 PDT; 35s ago

      Process: 524 ExecStart=/usr/bin/hciattach /dev/serial1 bcm43xx 921600 noflow - (code=exited, status=1/FAILURE)

     

    Jul 10 11:45:36 raspberrypi hciattach[524]: Failed to reset chip, invalid HCI event

    Jul 10 11:45:36 raspberrypi hciattach[524]: Can't initialize device: Success

    Jul 10 11:45:36 raspberrypi hciattach[524]: bcm43xx_init

    Jul 10 11:45:36 raspberrypi hciattach[524]: Flash firmware /lib/firmware/BCM43430A1.hcd

    Jul 10 11:45:36 raspberrypi systemd[1]: hciuart.service: control process exited, code=exited status=1

    Jul 10 11:45:36 raspberrypi systemd[1]: Failed to start Configure Bluetooth Modems connected by UART.

    Jul 10 11:45:36 raspberrypi systemd[1]: Unit hciuart.service entered failed state.

     

    This is the link I am following:

    https://www.raspberrypi.org/forums/viewtopic.php?f=28&t=148305

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jomoenginer
    jomoenginer over 10 years ago in reply to jomoenginer

    I have moved the EnOcean Pi 902 to a B+ Raspberry Pi and after some work to get the Serial port up running with the Pi 902, I was finally able to get some communication with the EnOcean Pi 902 from the serial bus.

     

    I ended up using minicom as well as a serial python script to see the input from the switch from the Switch Design Kit.  At least now I know the EnOcean Pi is working.  I'm still not able to enable the BLE device on the RasPi 3 as of yet so I will would like to resolve that.

     

    Screen shot from from the Pi 902 via minicom:

     

    image

     

    Screen shot from Fhem showing the EnOcean Device:

    image

     

    Next step is to get the EnOcean switch to control the iLumi BR30 and tie it all to OpenHAB running on the RasPi 3.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 10 years ago in reply to jomoenginer

    Okay, finally a bit of success.     After searching the web and attempting many changes to the RasPi 3 config, I finally stumbled on the needed info to get the On Board BLE device working again on the RasPi 3.  I am not sure what got it to the state it was in, but it is all working now.

    This is what I found:

    To fix the issue with the On Board BLE (hci0) not showing after an update on the RasPi 3, I followed the info in the following post, although I do not know what is being said:  (NOTE:  I have since found some of the info in other links but this one listed the steps more logically:

    http://www.fhemwiki.de/wiki/Raspberry_Pi_3:_GPIO-Port_Module_und_Bluetooth

     

    1. Edit /boot/config.txt and add the following:

     

          BLE Fix:

          sudo view /boot/config.txt

     

     

         # Additial overlays    

         dtoverlay=pi3-miniuart-bt

         force_turbo=1

     

     

         # Enable UART

         enable_uart=1

         #force_turbo=1

     

    2.  Edit /boot/cmdline/txt

    Add "core_freq=250" to the end of the cmdline string:

        dwc_otg.lpm_enable=0 console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 elevator=deadline fsck.repair=yes rootwait core_freq=250

     

    3. Edit "hciuart.service" change "ttyAMA0" to "ttyS0" if not already set.

         $ sudo view /lib/systemd/system/hciuart.service

     

     

         [Unit]

         Description=Configure Bluetooth Modems connected by UART

         ConditionPathIsDirectory=/proc/device-tree/soc/gpio@7e200000/bt_pins

         Before=bluetooth.service

         After=dev-ttyS0.device

     

         [Service]

         Type=forking

         ExecStart=/usr/bin/hciattach /dev/ttyS0 bcm43xx 921600 noflow -

     

    4. Add a "sleep 10" to the start section in the "fhem" init script if using FHEM.

        $ sudo view /etc/init.d/fhem

     

         case "$1" in

         'start')

                 echo "Starting fhem..."

                 perl fhem.pl fhem.cfg

                 RETVAL=$?

                sleep 10

                 ;;

     

    After performing these steps and rebooting the board, the on board BLE device should show up again:

    In my case I still had the USB BLE Dongle installed so both hci devices were listed in the hcitool listing from bluez:

          $ sudo hcitool dev

         Devices:

           hci1 B8:27:EB:0A:18:49  <-- On Board RasPi 3 BLE device

           hci0 5C:F3:70:6E:13:4B  <-- USB BLE Dongle

     

     

          $ sudo hciconfig

         hci1: Type: BR/EDR  Bus: UART

           BD Address: B8:27:EB:0A:18:49  ACL MTU: 1021:8  SCO MTU: 64:1

           UP RUNNING

           RX bytes:717 acl:0 sco:0 events:42 errors:0

           TX bytes:1560 acl:0 sco:0 commands:45 errors:0

     

        hci0: Type: BR/EDR  Bus: USB

           BD Address: 5C:F3:70:6E:13:4B  ACL MTU: 1021:8  SCO MTU: 64:1

           UP RUNNING

           RX bytes:4967 acl:44 sco:0 events:348 errors:0

           TX bytes:4942 acl:45 sco:0 commands:226 errors:0

     

    The /dev/serial* to tty mapping is now as follows:

    $ ls -lt /dev/serial*

    lrwxrwxrwx 1 root root 5 Jul 16 22:59 /dev/serial1 -> ttyS0

    lrwxrwxrwx 1 root root 7 Jul 16 22:59 /dev/serial0 -> ttyAMA0

     

    Looking at the Fhem messages, we can see the EnOcean Pi is still working:

     

    // Fhem messages

    Events:

    2016-07-16 09:56:31 EnOcean EnO_switch_002BA820 buttons: pressed

    2016-07-16 09:56:31 EnOcean EnO_switch_002BA820 channelB: B0

    2016-07-16 09:56:31 EnOcean EnO_switch_002BA820 A0,B0

    2016-07-16 09:56:31 EnOcean EnO_switch_002BA820 buttons: released

    2016-07-16 09:56:31 EnOcean EnO_switch_002BA820 buttons: released

    2016-07-16 09:56:33 EnOcean EnO_switch_002BA820 buttons: pressed

    2016-07-16 09:56:33 EnOcean EnO_switch_002BA820 channelB: BI

    2016-07-16 09:56:33 EnOcean EnO_switch_002BA820 AI,BI

     

    NOTE:  I found if Fhem init script was up and running, the EnOcean script would not display any events from the Pi device, thus I shut down the Fhem process prior to running the EnOcean script or before running the OpenHab start script. 

     

    pi@raspberrypi:~ $ sudo /etc/init.d/fhem status

    fhem is running

    pi@raspberrypi:~ $ sudo /etc/init.d/fhem stop

    Stopping fhem...

    pi@raspberrypi:~ $ cd EnOceanSpy/

    pi@raspberrypi:~/EnOceanSpy $ sudo ./EnOceanSpy /dev/ttyAMA0

    Starting EnOceanSpy...

    2016-07-16 10:05:14  55 00 07 07 01 7A F6 70 00 2B A8 20 B0 01 FF FF FF FF 30 00 E5

    2016-07-16 10:05:15  55 00 07 07 01 7A F6 00 00 2B A8 20 A0 01 FF FF FF FF 33 00 97 55 00 07 07 01 7A F6 10 00 2B A8 20 B0 01 FF FF FF FF 36 00 9E

    2016-07-16 10:05:16  55 00 07 07 01 7A F6 00 00 2B A8 20 A0 01 FF FF FF FF 34 00 FC 55 00 07 07 01 7A F6 37 00 2B A8 20 B0 01 FF FF FF FF 45 00 18 55 00 07 07 01 7A F6 00 00 2B A8 20 A0 01 FF FF FF FF 42 00 20

     

     

     

     

     

    If needed, Change the OpenHAB serial port setting to ttyAMA0:

    $ view configurations/openhab.cfg

     

         # EnOcean USB adapter serial port

         enocean:serialPort=/dev/ttyAMA0

     

     

     

    Initially, after doing all of this and seeing both the On Board BLE device working as well as the EnOcean device working, when I started OpenHAB, the PTM 210 U events were not being reported by OpenHAB.  However, I did find a blogpost posting by  Kai Kreuzer (The Creator of OpenHAB)  regarding this issue.

    http://kaikreuzer.blogspot.com/2014/08/forget-me-not-with-openhab-and-enocean.html

     

    He states:

    “…  Unfortunately, the RXTX library that is used by openHAB for connecting to serial ports does not consider /dev/ttyAMA0 to be a standard port and thus simply does not recognise it. You therefore have to explicitly declare it through the JVM parameter "-Dgnu.io.rxtx.SerialPorts=/dev/ttyAMA0" in the start(_debug).sh launch script.”

     

     

    I added the following heading:

      echo Launching the openHAB runtime...

      java \

      

        -Dgnu.io.rxtx.SerialPorts=/dev/ttyAMA0 \

     

     

     

     

     

    After this, I was able to see the events from the EnOcean Pi via OpenHAB again when pressing the PTM 210u switch..

     

    Messages from openhab.log:

    2016-07-17 01:33:23.303 [INFO ] [enhab.model.script.EnOcean Off] - Trying to run python script

    2016-07-17 01:33:23.315 [INFO ] [g.openhab.io.net.exec.ExecUtil] - executed commandLine 'sudo /usr/bin/python /opt/openhab/configurations/scripts/test2.py iLumi1 255 255 255'

    2016-07-17 01:33:23.317 [INFO ] [penhab.model.script.EnOcean On] - Send on

    2016-07-17 01:33:23.499 [INFO ] [enhab.model.script.EnOcean Off] - Trying to run python script

    2016-07-17 01:33:27.107 [INFO ] [penhab.model.script.EnOcean On] - Trying to run python script

    2016-07-17 01:33:27.118 [INFO ] [enhab.model.script.EnOcean Off] - Trying to run python script

    2016-07-17 01:33:27.126 [INFO ] [g.openhab.io.net.exec.ExecUtil] - executed commandLine 'sudo /usr/bin/python /opt/openhab/configurations/scripts/test2.py iLumi1 0 0 0'

    2016-07-17 01:33:27.128 [INFO ] [penhab.model.script.EnOcean On] - Send off

    2016-07-17 01:33:27.337 [INFO ] [enhab.model.script.EnOcean Off] - Trying to run python script

     

     

     

     

     

     

    Now, the only thing left is to get the EnOcean Pi to recognize other EnOcean sensors.  Thus, far I have not been successful with this, but that is something for a later time.

     

    I’ll create another post to outline how I am controlling the ilimi BR30 with the EnOcean PTM 210U via OpenhHAB.