• Products and Partners
    Products and Partners
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
Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog PiIoT - The perfect reading place #12 [tech]: SenseHAT interactive, the controller interface case
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
  • Author Author: balearicdynamics
  • Date Created: 31 Jul 2016 3:20 PM Date Created
  • Views 1981 views
  • Likes 7 likes
  • Comments 13 comments
  • controller
  • visually-imparied
  • internet of things
  • sensehat
  • piiot
  • gearbest.com
  • 3D Printing
  • 3d rendering
  • case design
  • raspberry pi
  • muzieum.nl
  • diginformale.it
  • lorenzo merlo
  • iot
  • interface
  • motion sensors
  • assembly
  • interactive
  • case
Related
Recommended

PiIoT - The perfect reading place #12 [tech]: SenseHAT interactive, the controller interface case

balearicdynamics
balearicdynamics
31 Jul 2016

A special case

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The position and motion sensors information from the SenseHATSenseHAT on the Raspberry PI3Raspberry PI3 together with the RGB 8x8 display are  the perfect tool to make the controller interactive interface for IoT project.

Making the device easy to control by any kind of user the hardware needs a case. The form design and the impacting bright yellow colour harmonise with the site where the installation will be set in place; it is also an easily identifiable object by visually-impaired users.

The following images shows the rendered design of the case hosting the PI3 and SenseHAT

imageimageimage

imageimageimage

The design has been split in two halves to include the hardware elements as shown below:

imageimage

Top and bottom parts will be fixed with 4 Parker screws. Based on the first tests the internal air circulation should be sufficient for Raspberry PI3 cooling.

3d printing and assemblilng

image

The 3D printing operation requires about 5 hrs total with a 0.4mm nozzle and a layer thickness of 0.2mm The case will not be stressed mechanically so it is sufficient setting the internal fill to 25% with a 0.6 thickness to the sides. As shown in the above image most of the time required depends on the need of a full internal support of the empty spaces.

imageimage

The above image shows the "kit" components ready for assembling; note the the open window for the SenseHAT LCD will be sealed with a 2mm opaline acrylic frame: this generates a nice effect for the display readability. The internal hardware does not need to be fixed with screws but a 5mm antistatic foam bed is sufficient, pressing the internal assembly when the screws are closed.

 

{gallery} Assembly steps

image

The components ready for assembly

image

The top side with the Raspberry PI3 fit in place.

image

The case ready to be closed

image

Closing the case with the four screws

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago +3
    Hi Enrico, That looks amazing, especially the curves, and it is practical too, with ventilation slots and everything : ) By the way, if you want to use M3 machine screws (bolts) instead of wood screws…
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz +1
    Hello Shabaz! Happy to see you aboard again I have already saw these in some industrial cases but I have hot though how to search them. Sometimes I loose a lot of time because I don't know the technical…
  • shabaz
    shabaz over 10 years ago in reply to balearicdynamics +1
    I've unfortunately not found a seller of M2 inserts like that, I too would like to obtain some. There is this manufacturer https://www.tappex.co.uk/multisert-inserts#selectors but they don't have an online…
  • shabaz
    shabaz over 10 years ago in reply to balearicdynamics

    I've unfortunately not found a seller of M2 inserts like that, I too would like to obtain some.

    There is this manufacturer https://www.tappex.co.uk/multisert-inserts#selectors

    but they don't have an online store.

    On aliexpress they have what is advertised as 'injection moulding nut' which is similar and is available in M2, however is more optimised for having plastic moulded around it, but I think would still work reasonably using the soldering-iron method (need a thin tip or file an old one, to fit the 2mm hole). I've use the 3mm injection moulding nut with soldering iron into sheet acrylic, and it stayed in ok.

    EDIT: this is how the M3 one (intended for injection moulding) looks after inserting with soldering iron:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to shabaz

    Hello Shabaz!

     

    Happy to see you aboard again image I have already saw these in some industrial cases but I have hot though how to search them. Sometimes I loose a lot of time because I don't know the technical name of some parts and also I have no idea where these can be found. Very good advice. In the case of this tool I should find M2 at least as the screws are very small, or enlarge the holes. But I should use these in this case and a lot of other. Great solution, really!

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago

    Hi Enrico,

     

    That looks amazing, especially the curves, and it is practical too, with ventilation slots and everything : )

    By the way, if you want to use M3 machine screws (bolts) instead of wood screws, I found a convenient way recently.

    I tried it with acrylic, but it would work with 3D printed stuff too.

    Basically, design in some holes, and then insert these brass heat sertsbrass heat serts. Perhaps press-fit is ok too, but

    I used heat to push them in (there are other inserts more optimised for press-fit). To do that, I just pushed them over the soldering iron

    (set to a temperature which results in the plastic gently melting, not too rapidly, so that you have time to position it correctly. It will slowly melt

    into the hole, and then just pull out the iron.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<