PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog AI powered CNC Painting Machine - Blog #1 - Idea
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
  • Author Author: Attila Tőkés
  • Date Created: 21 Mar 2019 8:31 PM Date Created
  • Views 1245 views
  • Likes 6 likes
  • Comments 3 comments
Related
Recommended

AI powered CNC Painting Machine - Blog #1 - Idea

Attila Tőkés
Attila Tőkés
21 Mar 2019

THE IDEA

 

I have some spare stepper motors and CNC parts, so I thought to build an AI powered Painting Machine using the Raspberry Pi.

 

The machine will work as follows:

  • a source image / photo is provided
    • the RPi Cam could be also used to take a photo
  • the image / photo is given to a AI algorithm to transform it to the style of a famous painter
    • inspiration
      You don't have permission to edit metadata of this video.
      Edit media
      x
      image
      Upload Preview
      image

      (source: Two Minute Papers)
    • white paper:

      Chuan Li, Michael Wand - Combining Markov Random Fields and Convolutional Neural Networks for Image Synthesis
      (https://arxiv.org/pdf/1601.04589v1.pdf)

 

  • the output image is sent to a Raspberry Pi controlled CNC painting machine, which will output the image to a piece of paper
    • I thought to try different approaches, to see which works better:
      • color pen based
      • laser engraving
      • 3D printing few layers
      • etc.

 

The frame I want to build using OpenBuild parts (aluminium profiles, bearings, wheels, belts). It will look something like this:image

(https://www.instructables.com/id/DIY-5500mW-Laser-Engraver-Cutter/ )

 

Bill of Materials
(preliminary list)

  • PiCasso Design Challenge: The Kit
    • Raspberry Pi 3 B+ (/starter kit)
    • Raspberry Pi Camera V2
    • PiFace Digital 2
  • 2 x NEMA 17 stepper motors (I have these)
  • 2 x lead screws (I have these)
  • extruded aluminium profiles, bearings, wheels, belts, etc for the free (need to purchase)
  • 2 x stepper driver (DRV8825)
  • 1 x servo motor (I have these)
  • laser module (i have some from DVD drivers)

 

Of sure, all the hardware and software parts of project will be fully open source.

WHAT'S NEXT?

 

Today I got the challenge kit. Here it is along with some CNC parts I had:

image

 

The next 2 blog post / steps, I think, will be:

  1. CNC Frame - find an open source CNC frame, suitable for the project; order parts
  2. AI Algorithm - find an implementation / try to reproduce the image transformation algorithm from the linked white paper

 

Cheers,

Attila

  • Sign in to reply

Top Comments

  • rddorris
    rddorris over 7 years ago +2
    I really like this project. You might consider using these brush pens... https://www.amazon.com/Watercolor-Flexible-Beginners-Coloring-Calligraphy/dp/B07KLZC6YW/ref=sr_1_7?crid=35YAFYWTHM4X7&ke…
  • dubbie
    dubbie over 7 years ago +1
    This looks very interesting. You could also try an air-brush if you want everything a but fuzzy. They do have some tendency to drip though. Dubbie
  • javahead
    javahead over 7 years ago +1
    Great project. Have you seen this: https://www.npr.org/sections/alltechconsidered/2016/04/06/473265273/a-new-rembrandt-from-the-frontiers-of-ai-and-not-the… As a painter, the medium adds to the 'painterly…
Parents
  • rddorris
    rddorris over 7 years ago

    I really like this project.  You might consider using these brush pens...

    https://www.amazon.com/Watercolor-Flexible-Beginners-Coloring-Calligraphy/dp/B07KLZC6YW/ref=sr_1_7?crid=35YAFYWTHM4X7&ke…

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rddorris
    rddorris over 7 years ago

    I really like this project.  You might consider using these brush pens...

    https://www.amazon.com/Watercolor-Flexible-Beginners-Coloring-Calligraphy/dp/B07KLZC6YW/ref=sr_1_7?crid=35YAFYWTHM4X7&ke…