PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog HoloPiBot # 1 : My Unofficial Entry
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
  • Author Author: dubbie
  • Date Created: 15 Mar 2019 8:48 AM Date Created
  • Views 1156 views
  • Likes 11 likes
  • Comments 9 comments
  • holopibot
Related
Recommended

HoloPiBot # 1 : My Unofficial Entry

dubbie
dubbie
15 Mar 2019

As I didn't want to be an official entry to this PiCasso challenge I have waited until the official contestants have been announced (well done to all of them) in order to avoid muddying the waters, so to speak. At the moment I'm still not sure what all of them will be doing so if any of my ideas clash just let me know and I'll do something else.

 

As I really like mobile robots (I really really like mobile robots) I wondered how to incorporate a mobile robot into this challenge. My idea is to make a holonomic mobile robot with a downward looking camera that is programmed to randomly move in the horizontal plane but maintaining its orientation. This would be placed over an art work, perhaps even a Picasso as I quite like some of his work, with a magnified image of the small portion of the picture captured by the camera being displayed on a flat screen video display carried on the top of the holonomic robot.

 

I have already been learning Pi (with my very old Pi B connected via Ethernet) and I have purchased some step motors and drivers in order to start creating the holonomic driving characteristic. I do have access to a proper PC display which has an HDMI input and also a 12V power input (I also have two lead acid batteries salvaged from a building fire alarm) but it might be a bit heavy for the motors. I had originally though of using a 5 inch or 7 inch display but that would mean purchasing one - which I might still do anyway. Then I hope to 3D print most of the structure holding everything together to make everything as smooth and pretty as possible. I might even spray paint some of it.

 

I'll have to see how it goes. I have to go now as I have three more shelves to put up.

 

Dubbie

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +4
    Dubbie, This sounds like an interesting project. I like how you bring frequently bring a robot to the party, as they do make parties better. Good luck! Gene
  • dixonselvan
    dixonselvan over 7 years ago +3
    All the best dubbie sounds like fun ... just to clear myself so your robot projects (magnifies) a small portion of an artwork?
  • three-phase
    three-phase over 7 years ago +3
    What! who on earth would insist on putting shelves up ahead of robot playing projects. Good luck.
Parents
  • dixonselvan
    dixonselvan over 7 years ago

    All the best dubbie sounds like fun ... just to clear myself so your robot projects (magnifies) a small portion of an artwork?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to dixonselvan

    Dixon,

     

    Yes, that's the plan, to display a magnified version of whatever the camera is seeing. I haven't done any image processing before (that is  - magnification) so hopefully I'll be able to do it. If I can get the magnification using a lense that would be easier.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago in reply to dixonselvan

    Dixon,

     

    Yes, that's the plan, to display a magnified version of whatever the camera is seeing. I haven't done any image processing before (that is  - magnification) so hopefully I'll be able to do it. If I can get the magnification using a lense that would be easier.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down