PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Pi Power Image
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
  • Author Author: armour999
  • Date Created: 24 Feb 2019 6:16 PM Date Created
  • Views 930 views
  • Likes 8 likes
  • Comments 4 comments
Related
Recommended

Pi Power Image

armour999
armour999
24 Feb 2019

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Wow this is beautiful and is a design by Dana Zelig. She is using a software package called Processing but does not indicate what hardware she is using. There is no copy write notice.

So this is exciting because the website  Processing for Pi provides all the tools to set this up on the Raspberry Pi B+ and Raspberry Camera. The website is here.

 

There is a image to download that includes the Processing  and libraries to quickly get you started. There are Tutorials to help you get started with the Raspberry Pi camera.

 

So the plan part 1 is to:

 

1, Write the image to Raspberry Pi 3+

2, Install and activate the Raspberry Pi camera

3, Follow the tutorial for Processing and the Pi Camera

4, Experiment and Create!

 

So Element14 has included in the kit the PiFace Digital 2 daughter board. If I can throw in some additional hardware from my workbench I am proposing to activate the Processing Sketch with a Reed Sensor. For now it would be if a door is opened.

 

image

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +2
    Very cool! I like using the EnOcean adapter to create triggers for your artwork. Good luck! Gene
  • beacon_dave
    beacon_dave over 7 years ago +2
    Sounds great. Monash University ran a MOOC on generative art using the Processing environment a couple of years ago which was interesting. The art of Casey Reas (one of the co-initiators of the Processing…
  • e14phil
    e14phil over 7 years ago in reply to beacon_dave +2
    Exciting!
Parents
  • genebren
    genebren over 7 years ago

    Very cool!  I like using the EnOcean adapter to create triggers for your artwork.   Good luck!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Very cool!  I like using the EnOcean adapter to create triggers for your artwork.   Good luck!

    Gene