PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - Kinetic Art Mobile - Post 3 - Will it go round in circles????
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
  • Author Author: genebren
  • Date Created: 26 Mar 2019 12:18 AM Date Created
  • Views 3090 views
  • Likes 14 likes
  • Comments 21 comments
  • 3D Printing
  • picasso_design_challenge
Related
Recommended

PiCasso Design Challenge - Kinetic Art Mobile - Post 3 - Will it go round in circles????

genebren
genebren
26 Mar 2019

Prior posts in the PiCasso Design Challenge:

PiCasso Design Challenge - Kinetic Art Mobile - Post 1

PiCasso Design Challenge - Kinetic Art Mobile - Post 2

 

In the lyrics of Billy Preston (Will it go round in circles), ... Will it go round in circles, will it fly high like a bird up in the sky? ...  It was my goal to find out.

 

Today I assembled and tested one of the rotating arm/orbs for my Kinetic Art Mobile. There is never an end to the ways in which a simple exercise can end up taking your whole day, but today was proof again that it can and it does.  I thought that I would embark on a simple experiment today.  I had all of the steps in my mind and I thought for sure, this is going to be easy. Ha!  Not quite so.

 

I have printed two separate halves of the my fan driven orb, each at a slightly different revision, but neither quite the final version.  In each orb half I mounted a fan.  I ran wires (individual 5 volt lines to each fan and a common ground) through all the support shafts and attach to the leads of the slip ring.  After several attempts to attach the wires I finally found the correct sequence (pivot ball first and outside orb second proved to be the most successful order).

 

imageimage

The image to the left is the original orb design.  The fan was attached with bolts and nuts through the housing.  This design broke up the sphere more and had some thin plastic edges that did not form well.  On the second image, the fans are retained by self tapping screws from within the orb.  The four slightly larger holes were additional air intake holes (that actually turned into exhaust holes - read more below).

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

I had assumed that I could achieve a balance with the orb 3 feet from the pivot and a counter weight attached 1 foot from the pivot.  I could not attach enough weight on the short rod to get the system to balance (I used a first run of the pivot design as a container for BB's and attached a short extension rod with 8 bearings), so I added a 1 foot extension and tried again.

image

The end of the initial 1 foot section of counter balance tube is at the extreme right hand side of the image.  The blue tap is sealing up the repurposed bearing/slip ring retainer housing that was filled with BB's.  At the left hand end of the modified counter balance shaft is a section of 7/32" brass tubing with 8 of the same bearings that are used as pivots on the main shaft.  This weight seems to have been enough to bring the assembly close to balance, but I was hoping to not need so much weight on the arms, as this will have a tendency to make the rotation of the obs sluggish with so dead weight in the rotating mass.  I think I will have to further extend the counter balance arms (maybe even longer that 3 feet) to lessen the weight needed to balance everything out.

 

 

I then mounted a temporary support arm to suspend the test assembly.  With the test arm attached to the support arm, I ran wires down to a lab power supply.

 

image

I the process of testing the movement of arm I noticed that while it would move in one direction, it would not move in the opposite direction.  This is when I noticed that I have to different fan types installed in the orb.  I had noticed different label colors (blue and green), but both labels had the same part number.  Closer inspection showed that the fans had inverse vanes, i.e. with the same direction of rotation one fan would blow and the other would suck.  I replaced one of the fans, so that each side of the orb now had the same fan type.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Here is a short video of the arm and orb moving in a clockwise (looking up) direction.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

And here is a short video of the arm and orb moving in a counter-clockwise direction.

 

The arm is moving far more sluggishly than I had hoped.  In closer inspection of the fans in the orb, it appears that I still might have the wrong fans in place.  I had initially tested one of the fans (green label???) which appeared to be exhausting air on the labeled end of the fan.  The orb currently has two blue labeled fans, which appear to be blowing air through the orb and exiting on the opposite side.  This is not the preferred direction, as this is pressurizing the orb and likely losing propulsion in the process (leaking out the orb seam and fighting the resistance of opposite fan vanes).

 

But, the good news is yes, It will go round in circles!

 

Thank you for following along on my little journey, more to come!

Gene

 

Update - 3/27/2019

I reversed the two fans (now exhausting  in the orb and retried the rotational tests.  The thrust seems improved and the orb more quickly accelerates in it rotation.  Reverse thrust braking and change of direction is also improved.  I also noticed that my makeshift support was still not quite level and the orb was actually going 'uphill' a bit at times.  Readjusting this also improved the startup speeds.  image

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +6
    Gene, Looks good despite the problems with the fans. It looks quite a bit like a death star. Air is slippery stuff to work with so this is pretty good. Will there be more orbs rotating at different levels…
  • fmilburn
    fmilburn over 7 years ago +5
    Hi Gene, I was slow to catch on but I finally get it :-) Looking very good... Frank
  • genebren
    genebren over 7 years ago in reply to three-phase +5
    Donald, It was good to see it moving! I did a very early test with the slip-rings and fans taped to the aluminum rod (with a counter weight), but as I was holding this up right over my desk, I was unable…
Parents
  • ralphjy
    ralphjy over 7 years ago

    Interesting project.  Look forward to reading about how you work through your issues.  I've wanted to try out these lower cost slip rings but haven't had the opportunity.  Seems like they are working for you. 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to ralphjy

    Ralph,

     

    Thanks for following along.  I am so far, very happy with the slip rings.  I had hoped to find a low cost slip ring with flanges on both sides, in order to get a more stable connections.  As it stands, I will need to glue the tiny rotor hub to the input tube and lightly clamp the stator side into the bearing retainer (spongy tape strips??).

     

    I have not put a scope on the stator side of the slip ring to evaluate the noise, but so far, so good.

     

    Thanks again,

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 7 years ago in reply to genebren

    You actually answered both questions I forgot to ask image

     

    I didn't see how you attached the rotor.  Glue works - I wonder how it's intended to be used?  Maybe a compression fit on both pieces?  Flanges would have been nice.

     

    If you get a chance to evaluate the electrical performance, I'm definitely interested.

     

    Ralph

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago in reply to ralphjy

    Ralph,

     

    I am not really sure how they intended for these to be mounted.  I must admit that I did a fair amount of head scratching, trying to figure out if these would work or not, but I took the plunge and ordered a few.  There are some with a single flange, which might have helped, but the flange was on the larger (less problematic) stator and not the tiny rotor.

     

    In the test videos, the rotor was just loose fitted inside the input shaft (no sleeve/glue).  My plan is to add a small sleeve (brass - OD = 3/16", ID = 5/32") inside the 7/32" brass tubing (OD = 7/32", ID = 3/16") near the rotor (with a slight flare added to allow the bearing to hold most of the weight).  The rotor is 4mm in diameter (0.15748"), this is only slightly greater than one thousandth of and inch smaller than the ID (0.15625" - delta = 0.00123").  In the final assembly, I will use silicone rubber to hold the sleeve to input shaft and the sleeve to rotor, as I want a small amount a flexibility against anything being out of round/center.  The stator will be compressed slighting inside the bearing retainer housing (pivot point). 

    imageimageimage

    As I get a little closer to a final assembly, I will instrument a test to measure the noise of the slip ring.

     

    Thanks again,

    Gene

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago in reply to ralphjy

    Ralph,

     

    I am not really sure how they intended for these to be mounted.  I must admit that I did a fair amount of head scratching, trying to figure out if these would work or not, but I took the plunge and ordered a few.  There are some with a single flange, which might have helped, but the flange was on the larger (less problematic) stator and not the tiny rotor.

     

    In the test videos, the rotor was just loose fitted inside the input shaft (no sleeve/glue).  My plan is to add a small sleeve (brass - OD = 3/16", ID = 5/32") inside the 7/32" brass tubing (OD = 7/32", ID = 3/16") near the rotor (with a slight flare added to allow the bearing to hold most of the weight).  The rotor is 4mm in diameter (0.15748"), this is only slightly greater than one thousandth of and inch smaller than the ID (0.15625" - delta = 0.00123").  In the final assembly, I will use silicone rubber to hold the sleeve to input shaft and the sleeve to rotor, as I want a small amount a flexibility against anything being out of round/center.  The stator will be compressed slighting inside the bearing retainer housing (pivot point). 

    imageimageimage

    As I get a little closer to a final assembly, I will instrument a test to measure the noise of the slip ring.

     

    Thanks again,

    Gene

    • Cancel
    • Vote Up +5 Vote Down