PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - PiMassive - Blog #10 - PiMassive is Alive!
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
  • Author Author: gam3t3ch
  • Date Created: 31 May 2019 10:34 PM Date Created
  • Views 5382 views
  • Likes 17 likes
  • Comments 22 comments
  • electronicartch
Related
Recommended

PiCasso Design Challenge - PiMassive - Blog #10 - PiMassive is Alive!

gam3t3ch
gam3t3ch
31 May 2019

Weighing in at 13.9lbs with 1,041,084mm of filament a grand total of 440hrs of 3d printing and CNC work a massive amount of painting time and cleanup the PiMassive is completed!

As promised here is video of my journey make sure to post any question below as well.  Let me know what you think!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

So a few things I didn't show along the journey was the final results with a few decals on it as well as the gpio working and VNC running so here you go some more photos to enjoy.

Once again this was a ton of fun and really taught me a lot thanks for checking it out and hope you enjoyed it!

 

image

VNC running on the pi I remoted in from computer changed the background to the glow of it needs a bit of resizing but not a big deal.

 

image

Lights off on the PiMassive and a few of our little friends chilling out and checking things out on it.  In the middle we have the size comparison to the product box the Raspberry Pi 3 B+ comes in.

 

image

Guess I should actually get the whole Pi in the picture as well.  As you can see on the left along the edge the LED light strip that is sticking out a bit I thought I gave it enough edge but guess not to hide it more.

How you like those decals on there?  Have the others but a bit too big so going to get those re-done to label the board more to make it more pretty.

 

image

Yup I like it!   but on to more comparisons scroll down a photo.

 

image

PiMassive VS Dad's Root Beer Bottle.

 

image

PiMassive VS DVD Case.

 

image

PiMassive VS a LaserDisc

 

image

And finally the SD Card adapter that came with the Raspberry Pi 3 B+

 

So as you can see in a few of the photos that there was a display outputting the voltage on the 3.3v GPIO Pin ill post in below here as well so you can have a closer look but its working. My battery for the Pi has been on for a few hours so not sure how much life is left in it so will have to do some other test to see the difference.

 

imageimage

So there we go might not have gotten as much done as I wanted or things go right the way I wanted them too but that was a massive amounts of trial and error and fun.

Thanks for checking out my project and following along with me I hope you enjoyed!

Take care and have a good day eh!

  • Sign in to reply

Top Comments

  • gam3t3ch
    gam3t3ch over 7 years ago +5
    Closer look at the scale of the USB Ports Got a call I wonder who it could be?
  • gam3t3ch
    gam3t3ch over 7 years ago +4
    giphy.com/.../iframe First attempt fail at getting all the colors will have to re-do it but so far whats your favorite?
  • dougw
    dougw over 7 years ago +3
    They sat bigger is better. Kudos on awesome El Grande PiMassive. They also say : If you are going to go .... go big.... and you definitely did. Congratulations on a great masterpiece.
Parents
  • dougw
    dougw over 7 years ago

    They sat bigger is better.

    Kudos on awesome El Grande PiMassive.

    They also say : If you  are going to go .... go big.... and you definitely did.

    Congratulations on a great masterpiece.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gam3t3ch
    gam3t3ch over 7 years ago in reply to dougw

    Thanks Douglas!  When I started I was worried something major would go wrong at the start if it did then I am not sure it would have been completed in time that's for sure.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to gam3t3ch

    Did you consider to show this pretty big at some maker fair?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gam3t3ch
    gam3t3ch over 7 years ago in reply to balearicdynamics

    I thought about it but closest one would be about a 7 hr drive as it wouldn't fit in a carry on that's for sure. the pictures really don't do the size justice everything looks like a miniature.  Maybe will have to send it to someone one day to have it shown. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gam3t3ch
    gam3t3ch over 7 years ago in reply to balearicdynamics

    I thought about it but closest one would be about a 7 hr drive as it wouldn't fit in a carry on that's for sure. the pictures really don't do the size justice everything looks like a miniature.  Maybe will have to send it to someone one day to have it shown.