PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - POV Globe Blog #9
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
  • Author Author: dwinhold
  • Date Created: 23 May 2019 2:36 AM Date Created
  • Views 1868 views
  • Likes 11 likes
  • Comments 8 comments
  • pov globe
  • picasso design challenge
  • dwinhold
Related
Recommended

PiCasso Design Challenge - POV Globe Blog #9

dwinhold
dwinhold
23 May 2019

Hello everyone

 

With the challenge coming to an end in just over a week it is time to post my 9th blog. I have spent the last week setting up the Raspberry Pi, electrical, testing power transfer through the bearings and creating a backup just in case it fails. I got the LED's up and running with the Raspberry Pi attached in place. The project is complete except for the final programming of my display. Below are pictures of the project built to completion and how it will look finished. The last blog will include the python code and video of the completed/running project.

 

This has been the most enjoyable project I have completed in a very long time. Thank you again to our sponsors, Element14 and the community.

 

image

 

image

 

image

 

Thank you for following

 

Dale Winhold

 

 

I had to include the below photo of my new toy.... 5.5W Laser CNC

 

image

 

 

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +3
    The final build looks good. What are you going to cut/etch with the laser head? DAB
  • dubbie
    dubbie over 7 years ago +2
    The laser looks good. Can it cut Perspex or is it just for etching? Dubbie
  • dwinhold
    dwinhold over 7 years ago +2
    With the cnc I plan on making my own printed circuit boards, apparently it works great for that. I have been engraving wood and cutting veneer with great accuracy. I have to experiment with different things…
Parents
  • dwinhold
    dwinhold over 7 years ago

    With the cnc I plan on making my own printed circuit boards, apparently it works great for that. I have been engraving wood and cutting veneer with great accuracy. I have to experiment with different things to see what it can do.

     

    Dale

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to dwinhold

    Dale,

     

    If it can etch PCB copper to make the tracks I would be very interested in that. When I did work I was told that lasers didn't work with copper clad board, makes sense as the light would be reflected, plus the gases given off would be very toxic. It was recommended to use a CNC router instead, which seemed to work fine, except it was very expensive (£30,000). I'd buy one (what else is my pension for?) but my wife says no. Maybe I can buy one a bit at a time! I also want a band saw (also no!) but I might get that, or a flat bed circular saw - I'm not sure which is best for me.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dubbie

    I suppose he is referring to the CNC. Laser – at least common laser cutters and engravers like this – can't engrave metals but to do this you need something more powerful like CO2 laser. Instead, the CNC router is perfect to make PCB

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dubbie

    I suppose he is referring to the CNC. Laser – at least common laser cutters and engravers like this – can't engrave metals but to do this you need something more powerful like CO2 laser. Instead, the CNC router is perfect to make PCB

     

    Enrico