PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog The project idea solidifies,
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
  • Author Author: therepairatrooper
  • Date Created: 16 Mar 2019 5:47 PM Date Created
  • Views 830 views
  • Likes 5 likes
  • Comments 1 comment
Related
Recommended

The project idea solidifies,

therepairatrooper
therepairatrooper
16 Mar 2019

I have been spending most of my free time and driving time mulling over the project. I have decided that how the monitor is framed is important to ensure that it has the look and feel of a real window. There are two challenges with this. Mounting the monitor flush in the wall would be ideal but not all construction situations are going to allow that as often basement walls might be 2x4 construction in front of a cement wall. So for this project I will focus on making an encompassing box that will look like a window frame but hang on the wall, much like a fireplace mantle. With a curtain rod and sheer curtains the feeling that this is a real window will be greatly amplified. The sill portion will allow the placement of knick-knacks to complete the effect. For the challenge I will be using a Sony 32" LCD, because I have that available and it is not my primary TV and will not cause my family grief.

 

I will use keyhole brackets to hold the box to the wall, which will create a tight fit and be very stable.

image

The top of the box facing the ceiling will have a perforated section to allow ventilation and prevent overheating. A small voltage fan with a temperature sensor will provide overheat protection.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +1
    Mark, Welcome to the element14 community. I see that you are jumping right in and taking on a design challenge project. Pretty cool idea. It is nice have a window (or simulated window) to allow you to…
Parents
  • genebren
    genebren over 7 years ago

    Mark,

     

    Welcome to the element14 community.  I see that you are jumping right in and taking on a design challenge project. Pretty cool idea.  It is nice have a window (or simulated window) to allow you to be a little more connected to your surroundings while you are sequestered in your cave.

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Mark,

     

    Welcome to the element14 community.  I see that you are jumping right in and taking on a design challenge project. Pretty cool idea.  It is nice have a window (or simulated window) to allow you to be a little more connected to your surroundings while you are sequestered in your cave.

     

    Gene