Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog S.H.E.L.F. - Plans and Ideas - Pi Chef Design Challenge - Blog post #1
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
  • Author Author: milosrasic98
  • Date Created: 19 Jan 2018 10:58 PM Date Created
  • Views 1966 views
  • Likes 8 likes
  • Comments 11 comments
  • pi chef design challenge
Related
Recommended

S.H.E.L.F. - Plans and Ideas - Pi Chef Design Challenge - Blog post #1

milosrasic98
milosrasic98
19 Jan 2018

For who is this project meant for (and how will it help)?

Ever went to the store and started thinking if you had some ingredient at home, or even worse came back home with your hands full of groceries ready to prepare that meal you've been wanting to make for so long just to see that you were wrong when you thought that you had that ingredient that you didn't buy? Or you just maybe want to keep track of how much something you consume. The idea of this project is to make a low cost smart shelf which would update you on your stock levels by sending the data to an Android app.

 

How will it work?

The center of the whole project would be the Raspberry Pi as the central brain which will communicate with the sensors and the internet. The shelf itself will be supported with scale sensors which will keep track of the weight, while a camera module above will monitor what is put on the shelf itself. To identify the different things on the shelf the most likely route for something like that would be either stickers for the packaging or specially designed containers (the progress of the project will determine). The idea of the stickers is to have cheap intuitive stickers of what is what, which would be recognized by the camera module. Of course making a sticker for everything would be impossible so the user will be able to match "blank" stickers to the desired thing using the app (By blank - the stickers will be universal; for example a number a person can read with the symbols around which would help the camera module). The user could print out there whenever he runs out. The other idea is having specially designed containers with some sort of sensor detecting what that is (Strict location for an ingredient for example). How the project and time work out will determine the way that I'll develop the project. The idea is also to make it possible to connect it to other shelves like this and adding other features that could be lights, smoke and temperature sensors, or anything else that would help around the kitchen. If this all goes well, the finishing part would be a heavy duty storage area, which would house vegetables with climate control (temperature, humidity, fresh air).

 

image

 

This is just a fast picture I made, and not close to the final design, I will have 3D models when i finish designing it

 

image

 

Some of the bigger challenges with the project

  1. Making the whole user friendly
    • Making it easy to use
    • Making it robust for everyday use
    • Making it easy to clean/assemble/disassemble
  2. Working with the camera and the stickers
  3. Making it low cost
  4. Multiple shelves working in tandem

 

 

Things that need to be done (probably will change with time)

  1. Completing the design (most of it done)
  2. Gathering the materials (need to get the scale sensors and the raw materials themselves like wood)
  3. Simple Android app (will have a list of items with how much is left)
  4. Sending data to the web via Raspberry
  5. Connecting everything (Android-Internet-Raspberry-Arduino-Sensors)
  6. Sensor calibration
  7. Computer vision
  8. Making and testing the computer vision with the stickers
  9. Building a first prototype
  10. Troubleshooting
  11. Adding features

 

In the end I would just like to say congrats to all the starter kit winners and to wish good luck to everyone!!! Unfortunately I didn't have much time to actually start doing anything more serious except gathering some of the stuff, it's the finals week for me at university so it's pretty fun here! Thanks for reading the post and if anyone has any comments on what's bad/good/something they would add, I would love to hear it!

 

Milos

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +6
    Milos, I have always wanted to do something like this. I have tried to sell my wife on how great this would be, so you would know your kitchen inventory, but alas, she does not think it would make her…
  • beacon_dave
    beacon_dave over 8 years ago in reply to dixonselvan +3
    This is a language barrier thing. Over here you can 'sell an idea' to someone which basically means you manage to persuade them to agree with your idea even if they were initially against it. I don't think…
  • e14phil
    e14phil over 8 years ago +3
    Hi Milos, W elcome to the challenge, as non sponsored challengers you are still entitled to be in the running for Winner and/or Finisher Prizes by using the Raspberry Pi, posting your 10+ Blogs in the…
  • dixonselvan
    dixonselvan over 8 years ago in reply to milosrasic98

    Thanks milosrasic98 for your explanation. I will follow up as you progress to understand things better image If you have time at the end, I suggest you can try with NFC tags as you have NFC expansion board at your disposal instead of the sticker system.

     

    NFC stickers come at around $10 - https://www.amazon.com/Black-NFC-Stickers-NTAG213-Tagstand/dp/B00KSR0636/ref=pd_lpo_vtph_107_lp_t_2/143-3658771-1781553?…

     

    Dixon Selvan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • milosrasic98
    milosrasic98 over 8 years ago in reply to genebren

    Thanks a lot for the good wishes genebren!!!

     

    Milos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • milosrasic98
    milosrasic98 over 8 years ago in reply to dixonselvan

    Hi dixonselvan

     

    As I have said the design isn't final yet, though i believe with the camera above I'll be able to get a good view of the shelf. I was thinking about the interactive display,  but I am not sure, on one hand it would make easier setting/ changing some stuff directly, on the other hand it will make the thing more cluttered and bulkier, my idea is to able to control everything you need by using the app. The easiest scales for me to get the hold of are the big ones which would measure the weight of the whole shelf, it's cheaper than having individual scales, also not everything has a container which is another issue. Not barcode exactly, barcode isn't intuitive, you don't know what it is, also to read barcode you need to get pretty close the sticker itself, my idea is making my own style of stickers (for example let's say a bright pink star, you could recognize the color and the shape of it, and would remember easier what it is than a barcode - of course the goal is to make stickers as unique (and intuitive) as possible so that the packaging of some of the products doesn't trigger the camera). Thanks a lot on the feedback and ideas!!!

     

    Milos

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 8 years ago

    Hi milosrasic98

     

    The camera module seems be fixed and I am not clear how it will be able to scan all the contents in the shelf. Next I suggest you can also include an user interactive display nearby the shelf.

     

    Also not sure why the entire weight of the shelf is measured when things will be kept in separate containers. When it comes to stickers and global numbers do you mean barcode?

     

    I like this shelf inventory concept. All the best for you to complete this project.

     

    Dixon Selvan

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 8 years ago in reply to genebren

    genebren  wrote:

     

    Milos,

     

    I have always wanted to do something like this.  I have tried to sell my wife on how great this would be, so you would know your kitchen inventory, but alas, she does not think it would make her life easier.  Oh darn!

     

    Good luck on your project!

    Gene

    genebren Hope you meant ‘tell’  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>