Products
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
Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Alternate Solution for Costly USB Microphone
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rushikesh988
  • Date Created: 6 Feb 2014 6:44 AM Date Created
  • Views 1837 views
  • Likes 2 likes
  • Comments 6 comments
  • microphone
  • cheap
  • usb
  • raspberry-pi
  • solution
  • rocking_pi
Related
Recommended

Alternate Solution for Costly USB Microphone

rushikesh988
rushikesh988
6 Feb 2014

Since our raspberry is not having microphone input port,we need to use USB interface for taking audio input. There are some USB microphones available in market but I found that these microphones are very expensive. But there is a good alternative solution to this problem.

 

          USB  SOUND CARD:

image

USB sound "cards", sometimes called "audio interfaces", are usually external boxes that plug into the computer via USB. A USB audio interface may describe a device allowing a computer which has a sound-card, yet lacks a standard audio socket, to be connected to an external device which requires such a socket, via its USB socket.

The USB specification defines a standard interface, the USB audio device class, allowing a single driver to work with the various USB sound devices and interfaces on the market.

Even cards meeting the older, slow, USB 1.1 specification are capable of high quality sound with a limited number of channels, or limited sampling frequency or bit depth, but USB 2.0 or later is more capable.(Source Wikipedia)

 

I found this device on shopclues  which is costing around Rs.169 , It is very good solution to our problem.

 

 

There are some other variants of this converters available online

Quantum QHM 623 USB Sound Card

SRA Sound Card USB S1 USB Laptop, Computer

USB Sound Card

USB SOUND CARD 7.1 CHANNEL SOUND

imageimageimageimage
Rs.148 on FlipkartRs.250 on FlipkartRs.174 on shopclues
Rs. 109 on ebay
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Thank you very much for the details.
Parents
  • babusingh9211
    babusingh9211 over 12 years ago

    Hey,
    I used these sound cards.
    but in mine case there is noise problem when interfaced with RPi,

    It worked fine with Windows.
    Do you have any idea about this?

    I used arecord & aplay to record and play recorded sound in RPi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rushikesh988
    rushikesh988 over 12 years ago in reply to babusingh9211

    I don't have much idea about this problem but I can suggest you to try using external powered USB hub.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • babusingh9211
    babusingh9211 over 12 years ago in reply to rushikesh988

    Have you used this?

    And may be your Idea of savings flopped when talking about powered USB hub image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rushikesh988
    rushikesh988 over 12 years ago in reply to babusingh9211

    A I  mentioned previously I don't have much idea about it, but I had the same problem ( USB peripheral not working properly) with wireless card in my previous project which got solved by using external powered USB Hub. External powered USB Hub cost only 150 rupees combining it with USB sound card cost still becomes cheap solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rushikesh988
    rushikesh988 over 12 years ago in reply to babusingh9211

    A I  mentioned previously I don't have much idea about it, but I had the same problem ( USB peripheral not working properly) with wireless card in my previous project which got solved by using external powered USB Hub. External powered USB Hub cost only 150 rupees combining it with USB sound card cost still becomes cheap solution.