Products
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
Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Raspberry Pi and Karaoke 2nd Week
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: babusingh9211
  • Date Created: 15 Feb 2014 4:48 PM Date Created
  • Views 805 views
  • Likes 3 likes
  • Comments 1 comment
  • raspi
  • rockingraspberrypi
  • raspberry-pi
  • rpi
  • rocking_pi
Related
Recommended

Raspberry Pi and Karaoke 2nd Week

babusingh9211
babusingh9211
15 Feb 2014

Hi,

I am excited to tell you about that I received my kit on this week’s Wednesday. It was like a gift for me in this valentine’s week ;).

image

 

The box contain Raspberry Pi Model B 512MB version, Pi Face and Display, Wi-Pi and 8GB SD card pre-installed with NOOBS.

image

Raspberry Pi

image

 

As everyone my family, friends and neighbours who see this asked me few questions like, What is this?, How it helpful?, What is its application?, Why to use only this?.

 

What is this?
This is Raspberry Pi, a credit card sized computer which is capable of perform most of the task which an ordinary computer can perform.
Moreover this can be used to interfaced this with digital sensors, display etc

 

How it is helpful?

It can be used with most of displays like ordinary TV, Monitors, HDTV and LCD. Also this can be helpful for creating & editing documents, programming, HD media solution with internet connectivity and lot more things.

 

What is its application?

It can be used to convert ordinary TV into smart TV in digital age. It can be used to create a robot, a data logger, a web browser and alot which a computer can do.

 

Why to use only this?

Best and simple reason is because of its cost. Apart from that a low powered device which can be operational at standard mobile charger. And moreover it extra features in small budget.

 

Pi-Face Control and Display

imageimage

It is device which allows users to use and control raspberry Pi without monitor and keyboard which significantly removes the use of other display making the device handier to use and saves power.
The Pi-Face CAD has onboard 16x2 LCD display and 5 tactile switches for input which removes the use of keyboard and Display for small application. Moreover to this it has IR remote transceiver which is helpful for controlling it with ordinary IR remote wirelessly using simple lirc libraries in RPi.

 

Wi-Pi

image

Fullscreen contentimage_29859.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

Wi-Pi is specially designed for Raspberry Pi for connecting it wirelessly with WLAN devices. It is cost effective USB module which connects it with Wi-Fi local area network. Wi-Pi uses the latest 802.11n Wireless Technology, and can support data rates of up to 150 Mbps, compared with older 54 Mbps 11g products. It also benefits from a higher wireless LAN bandwidth, making data transmission more efficient.


Pre Installed SD Card with Noobs

Fullscreen contentimage_29860.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>
Fullscreen contentimage_29861.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

I have received the 8GB class 4 memory card with preinstalled NOOBs. It allows users to install varieties of OS among Raspbian, RaspBMC, Pidora, RISC OS, Arch Linux and OpenELEC. Installing these OS is very easy task and has just few steps to follow.


What Extra things I need to use Raspberry Pi

 

For using the Raspberry Pi I need few more important things like a micro USB adopter. It is not so costly and also a mobile charger can work with it but a small condition that for Raspberry Pi model B it should be more than 800mA. But I found that too in my home.

Another is a power USB hub. It is not that important but it can be useful when connecting more than 2 USB devices. A simple hub can also do this task but because of low USB power efficiency of RPi power USB hub might be important. I have ordered that one from snapdeal.


image

 

For now, this is enough for the beginning. At last see what I’ve assembled with this all.

image

 

Regards,

Sumit Rai

  • Sign in to reply

Top Comments

  • mmohit00007
    mmohit00007 over 12 years ago +1
    buddy m very happy for you now u should work hard for the competition and i want u win
  • mmohit00007
    mmohit00007 over 12 years ago

    buddy m very happy for you now u should work hard for the competition and i want u win image