Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Road blocks to Karaoke
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bharatrai888
  • Date Created: 26 Apr 2014 4:36 PM Date Created
  • Views 2485 views
  • Likes 0 likes
  • Comments 14 comments
  • rockingraspberrypi
  • karaoke
  • rocking_pi
Related
Recommended

Road blocks to Karaoke

bharatrai888
bharatrai888
26 Apr 2014

Hi Friends,


In previous post I write about the use of raspberry with wolfson pi. I talked about the usage of the wolfson.


If talking about the karaoke which is our main target the raspbian fails as I already said in my starting post. Whereas the RaspBMC provide lag free music and video playback which is our main motto. As we all use it as karaoke which means using raspberry pi as media device.


So according to my experience and point of view the RaspBMC is best solution for this.


So for this I first backup my Raspbian data and restored my RaspBMC image which used to backup earlier.


And again it was the awesome feeling while playing lag free media.


Again going through each setting of raspbmc I also found the karaoke option inside the RaspBMC settings option.


At this point I enabled the option but while playing .kar file it fails.


Looking for the solution on the internet I found to put the soundfont.sf2 file and a blank timidity in the timidity folder which is located in ~/.xbmc/userdata/


I do the same but still it fails to open midi files. Looking inside the error log I compared it with the XBMC windows version logs. I found that there is no line containing timidity in the RaspBMC error log.


Other than that the initial idea which I have planned is working.


I am still searching for the proper solution which may help in playing midi files in RaspBMC.


Otherwise I’ll come up with initial idea to use raspberry pi as fully controlled karaoke machine.

  • Sign in to reply
Parents
  • cstanton
    cstanton over 12 years ago

    Isn't RaspBMC based on Raspbian and so you can just use the package which ragnar.jensen made to replace the kernel/install modules ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bharatrai888
    bharatrai888 over 12 years ago in reply to cstanton

    I haven't tried to replace the kernel/install modules. image

    I know both based on debian but still I am not sure to use it with RaspBMC as there is no documentation available and other information on internet.

     

    -- Bharteindu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • bharatrai888
    bharatrai888 over 12 years ago in reply to cstanton

    I haven't tried to replace the kernel/install modules. image

    I know both based on debian but still I am not sure to use it with RaspBMC as there is no documentation available and other information on internet.

     

    -- Bharteindu

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • cstanton
    cstanton over 12 years ago in reply to bharatrai888

    So what I'm suggesting is, setup your SD Card with RaspBMC.

     

    Once that's done, you can follow the steps here:

     

    Re: Re: Wolfson modified Noobs raspbian zipped img  Cannot unzip new download

     

    Which basically means you extract the file to / on the SDCard and edit config.txt to point to the kernel that was extracted.

     

    Does this make sense? Is that sufficient documentation for you ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bharatrai888
    bharatrai888 over 12 years ago in reply to cstanton

    Ok,

    Let me give it a try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 12 years ago in reply to bharatrai888

    If/when you get it booting with Ragnar's wolfson kernel, the next trick will be executing the usecase script / setting raspbmc to use the correct alsa reference value (which I think is in the usecase script but I'm sure ragnar.jensen is better versed in handling alsa than I.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bharatrai888
    bharatrai888 over 12 years ago in reply to cstanton

    I tried the step replacing kernel and installing some modules, and also I executes the use_case_scripts setting and tried all output ports. But still I am not getting output from the wolfson. After this I replace .asoundrc provided by the ragnar.jensen

    Also I tried in RaspBMC setting and set audio output to all devices. Even this step fails.

     

    Another thing after replacing kernel and installing libraries my booting time of RaspBMC is affected it takes too much time to boot up.

    ragnar.jensen please help me. Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 12 years ago in reply to bharatrai888

    Unfortunately I don't have the hardware in front of me at the moment to check the correct settings; but if you're having trouble with the RaspBMC installation and you have the time, the other way to attempt it is to have the Wolfson image from the element14 site, if you have it and know that it works, then build RaspBMC on top of it: RaspbianXBMC - Raspbian though it depends where the problem lies.

     

    Though I wonder if it's having a similar problem to Wolfson now working with pulseaudio and is outputting on the raspberry pi instead?