Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Rocking The Rocking Raspberry Pi Challenge.. Part 1 - A Over View Of Hardware & Problems..
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: saurocksall
  • Date Created: 6 Feb 2014 8:08 PM Date Created
  • Views 1382 views
  • Likes 2 likes
  • Comments 11 comments
  • rocking-the-rocking-raspberrypi-challenge
  • rockingraspberrypi
  • raspberry-pi
  • raspberrypi
  • rocking_pi
Related
Recommended

Rocking The Rocking Raspberry Pi Challenge.. Part 1 - A Over View Of Hardware & Problems..

saurocksall
saurocksall
6 Feb 2014

This is my first blog post for the Rocking Raspberry Pi Challenge, in this i will be writing about the hardware that I will receive, some problems which i will need to overcome and some other things in general. As this is a challenge i will not be telling every thing than i an planing to do in the first post it self, its just going to be a over view of things..

 

 

So lets take a look at the hardware that i will getting for the challenge :

 

Raspberry Pi Model B With 520 MB RAM :

                                                             image

The RPi is a great piece of hardware for making such projects / prototypes, it will provide the processing power and lots of input output ports, and it's high speed internet capabilities will be very useful for playing songs off YouTube..


 

8 GB SD Card with NOOBS :

                                                    image

The NOOBS or New Out Of Box Software on the card will be very a nice addition as I will not have to download NOOBS which is about of 1.3 GB, if any one of you want to download it click HERE. NOOBS has 6 operating systems ( Raspbian, RaspBMC, Pidora, RISC OS, Arch Linux and OpenELEC ) in it ready to be installed just with a click !! and even re-installing and changing the OS is as easy as installing it you just have to press and hold the SHIFT key when RPi is booting up and it will take you to the instillation setup, How cool is that !!


Learn More About It HERE.


Wi-PI :

                                                     image


Wi-Pi is the WLAN USB module RPi from Element14 it connects RPi to a Wi-Fi local area network, giving it a wireless internet connection it supports data speeds of up to 150 Mbps.


Learn More About It HERE.


PiFace Control & Display :

                                                                               image

It is a great add-on to the RPi because it can be used as a input / output device, and we no more need connect Pi to the monitor at least for basic tasks, i am looking forward to the portability factor for the Karaoke machine, and it provides me the power to do so, I have some other great ideas for the inputs which I wont be discussing in this post for obvious reasons.. Some key features of the PiFace Control & Display are 16X2 LDC with green back light, IR receiver, 3-position navigation switch, 5 tactile switches. Again i would like to say that its a great addition to the RPi, as it adds many features to the Pi..


Learn More About It HERE.

 

OK that's it about the hard ware that all of us contestants are getting for the challenge, Besides that we would need some more hardware for the project..


1 ). A HD TV or computer monitor (at least for the first boot- up ), then any analog monitor can be used.

2 ). A HDMI cable (for connecting the Pi to the HD TV or Monitor ).

3 ). Speakers ( if one is using a computer monitor which usually don't have in built speakers ).

4 ). A USB Microphone ( which I am unable to find till now ).

5 ). A Micro USB power supply for powering up the Pi, ( I will use a Mobile Phone Charger for that they usually have a output of 5 Volts and 1 Amp )


There are some other things that i intend to use, i wont be disclosing in this post. Now Let,s talk about some of the problems that all the contestants will face..

 

1 ). Till now I am unable to find a affordable USB microphone on the internet and in the local shops, a solution as suggested on the internet is to use a USB Sound Card Adapter. 

                                image

I did some research on the web and found that these things don't work properly even with Windows, so i seriously doubt that it will work with Pi, and even if it works i don't think that sound quality will be that good, and it will not also not look, its a matter of testing. if it works with the Pi and if the sound quality will decent i will do some hardware hacking to make it look good, these things are very cheep so i can risk that. That is if I cant find a Decent and affordable USB Mic, ill keep looking for a couple of more days..


2 ). Another problem for me is to make it as portable as possible, that is a big concern for me, I would love to take it to parties etc. I think that i will have to design a custom case or some thing for it, but i want to keep it pocket friendly..

 


OK that's it for now, i did not wrote about any software stuff as it not a big concern for me at the moment, i will write about it as i start to build the project in coming weeks, hope the Raspberry Pi and others are delivered to me in next 5 days, it would make the post more interesting as i have some awesome ideas if it does, wont tell it OBVIOUSLY.....image

 

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Good post, You should look for the USB Mic in your market, some computer shop owners keep them.. I also applied for the challenge but didn't got selected, bad luck of mine, i have worked on raspberry pi…
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    You should have told some of your plans buy BVIOUSLY.... Well written by the way, good work dude.
  • DAB
    DAB over 12 years ago +1
    Good post, I look forward to seeing your progress in setting up your project and get it operating. DAB
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    nice post dude, i to applied but didn't get selected.image

    i you did some research there, will keep following you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago in reply to e14 Contributor

    Thanks it feels good when people appreciate my work..... Keep following lots of secrets to be revealed soon...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • saurocksall
    saurocksall over 12 years ago in reply to e14 Contributor

    Thanks it feels good when people appreciate my work..... Keep following lots of secrets to be revealed soon...