Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Rocking The Rocking Raspberry Pi Challenge.. Part 8 Problems I am Facing With Wolfson Audio Card...
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: saurocksall
  • Date Created: 22 Apr 2014 8:35 PM Date Created
  • Views 2652 views
  • Likes 0 likes
  • Comments 12 comments
  • wolfson
  • rocking-the-rocking-raspberrypi-challenge
  • wolfson-audio-card
  • rockingraspberrypi
  • raspberry-pi
  • wolfson-pi
  • rocking_pi
Related
Recommended

Rocking The Rocking Raspberry Pi Challenge.. Part 8 Problems I am Facing With Wolfson Audio Card...

saurocksall
saurocksall
22 Apr 2014

Hi Guys, Sorry for the delay My exams are going on currently, so I was busy in them and had no time to write the blog, however I took time to work on the project,

In this post I will discuss about some problems I am facing with the Wolfson Audio Card.. If any one out there can help me please help me out..

 

So Here it goes..

 

First I tried to download the Image file provided by  Wolfson, it took around 15 hours to download, and after I unzipped the file size was bigger than the size of my memory card, I was depressed and angry because of this, So I searched and searched the internet for a solution for this and found ragnar.jensen's Image file which was smaller and I downloaded and installed on my card..

 

After which I am facing these problems :


1). Raspberry pi hangs allot, and gets over heated..


2).Wi-Pi and other USB devices don't work properly, works for some time and then stops completely and then system freezes..


3). When I remove and replace any USB device, Raspberry pi gets restarted, this is strange !!!


4). VLC Media player hangs allot, and shows error in audio output..


5). And the most interesting one is now I can't even get audio output form the Pi's audio jack !!!


The competition is near its end and I am now really far behind because of Wolfson Audio card, I am not a software person, but know the basic stuff, But unlike the PiFace CAD Wolfson Audio card has almost no support and tutorials etc. for making it easy to use, I agree that it is a fine piece of hardware but if it not easy to use its not worth any thing, the Element14 team should really need to focus on to provide some good documentation on how to use it, with some good examples like the PiFace People made, Something like that will be really helpful, and please make a smaller image file for it, or better make it install-able by apt-get or something..


If some one has the solutions to my problems please help me out, I will be really thank full to you guys...

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 12 years ago in reply to saurocksall +1
    Hi Saurabh, I think VLC lag is to be expected (or, more likely) if the video is of high bitrate or of particular encodings maybe. Could you try a low-res, small file that you store on the SD card, not…
Parents
  • cstanton
    cstanton over 12 years ago

    Hi Saurabh,

     

    after I unzipped the file size was bigger than the size of my memory card

     

    • What is the size of your memory card ?
    • What class is your memory card?
    • What image are you running on your memory card, if not the Wolfson one ?

     

    If the SD Card is less than a Class 6 then that's a problem which needs to be fixed, Christian tells me you were sent an 8gByte SD Card with NOOBS on it, that should be enough to have the Wolfson Audio Card image written to it (are you using Win32Imager as stated in the User Manual ? Wolfson Raspberry Pi Soundcard Manual (.IMG install) V1.1).

     

    Just to state the obvious you do not directly copy the .img file you download to the SD Card.

     

     

    Raspberry pi hangs allot, and gets over heated..

     

    You will probably find that if you get a new SD Card with a higher Class rating that the majority of your crashes will stop or you will have different problems.

     

    The default Wolfson SD Card Image that you can download from element14 overclocks the Raspberry Pi by default, so you could prevent that if you're using it by just removing those lines from the config.txt (overclock details here: RPiconfig - eLinux.org or here How to Overclock Your Raspberry Pi - Make Tech Easier ).

     

    Also it could be that your power supply isn't up to task; don't run it from a USB port on your computer, use a standalone power supply rated to at least 1Amp, preferably 2Amp.

     

    Failing that, put a heatsink on it. Even if its a few copper coins (I used to do that with my Playstation 2 slimline as a heatsink).

    Wi-Pi and other USB devices don't work properly, works for some time and then stops completely and then system freezes..

     

    This will be related to your SD Card and power as stated above.

     

    When I remove and replace any USB device, Raspberry pi gets restarted, this is strange !!!

     

    This is normal behavior, the Raspberry Pi does not handle USB very well and the Ethernet adapter shares the same chip. My experience has been that it reboots if it is a device that is power hungry (though not out of specification for the device, just something like a WiFi adapter).

     

    VLC Media player hangs allot, and shows error in audio output..

    It would help to copy and paste the errors into a quote on your blog post, but I suspect that this is related to the above issues, namely which SD Card image you're running and the Class of the SD Card.

     

    And the most interesting one is now I can't even get audio output form the Pi's audio jack !!!

    This could be down to any multitude of reasons, it makes sense that if you've got the Wolfson Audio Card and you've used a 'use case' it will have switched the audio output to your Wolfson Audio Card and that this would have to be changed. What the original settings are? I'm not certain. Typically it's easier to just wipe the SD Card and start again.

     

     

    Wolfson Audio card has almost no support and tutorials etc. for making it easy to use

     

    I understand it's my own blog post, but if you are just using Raspbian then the steps I point out here: Can you hear the Wolf(son) calling? Setting up and using the Wolfson Audio Card are relatively straight forward.

     

    The user manual is also a helpful resource to read thoroughly: Wolfson Raspberry Pi Soundcard Manual (.IMG install) V1.1.

     

    Frankly it sounds like the SD Card you're using is what is mainly hindering you if the Class rating is below 6. If you're having problems downloading SD Card images in future, let me know and I'll look at providing a mirror for the file(s) temporarily.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago in reply to cstanton

    Hi Christopher,

     

    Thanks for your help, I checked the power supply it is working find its already 5 volts 2 amps supply, I also tried another supply but the same problems occur, Over heating still is one of the problems, even though i have heat sinks on my PI, you ca see that in this image..

    Fullscreen contentimage_176481.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

    I am running the image file made by ragnar.jensen for the Wolfson pi..

    Raspberry Pi works fine without the Wolfson audio card and the USB problem is because of the Wolfson card only... I was able to play music with VLC media player out of the pi's audio jack but that was with NOOBS installed Raspbian on anther card..

    The NOOBS SD card we received was a 8 GB class 4 card i think its the main reason for the problem, now i need to buy a new card image  that is a problem as i have only a few days left for the challenge to end, what should I do now ??

     

    VLC  media player installed on the card with Wolfson pi image installed gives error " Audio output failed: The audio device "default" could not be used: No such device. "

     

    Please help me....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to saurocksall

    Hi Saurabh,

     

    I think VLC lag is to be expected (or, more likely) if the video is of high bitrate or of particular encodings maybe. Could you try a low-res, small file that you store on the SD card, not on USB stick or network? If that still causes lots of lag, try it on a USB stick?

     

    The Wolfson Pi card has no interaction with USB, but for now just don't unplug any USB device, to work around this.

     

    That then leaves the issue of "audio output failed" using VLC. Does that occur without the Wolfson pi card installed?  Did you try it with the

    Wolfson pi card plugged in? I'm still concerned that you're using an image that is not greatly tested (no disrespect to Ragnar's image - this should

    be fine in theory), but since you have an 8GB card, is there no official image that supports the Wolfson card?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 12 years ago in reply to saurocksall

    Hi Saurabh,

     

    I think VLC lag is to be expected (or, more likely) if the video is of high bitrate or of particular encodings maybe. Could you try a low-res, small file that you store on the SD card, not on USB stick or network? If that still causes lots of lag, try it on a USB stick?

     

    The Wolfson Pi card has no interaction with USB, but for now just don't unplug any USB device, to work around this.

     

    That then leaves the issue of "audio output failed" using VLC. Does that occur without the Wolfson pi card installed?  Did you try it with the

    Wolfson pi card plugged in? I'm still concerned that you're using an image that is not greatly tested (no disrespect to Ragnar's image - this should

    be fine in theory), but since you have an 8GB card, is there no official image that supports the Wolfson card?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • saurocksall
    saurocksall over 12 years ago in reply to shabaz

    Hi Shabaz,

     

    There is an official image but it is a 4.5 GB download and after unzipping it exceeds the size of a 8 GB card..

    and the video file i tried  to play was a mp4 file, resolution was 640 * 360, bit rate was 447 kbps, 25 frames a second..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to saurocksall

    Hi Saurabh,

     

    I see. What is the URL of the 4.5GB image? Are you unzipping on a Windows PC or something else? Also, I see someone has instructions to cross-compile, but even experienced software people may not want to go down that road if there is an alternative. Saurabh, if you have many hours to spare :-( there is the native compile method here Instructions for compiling the wolfson audio card kernel drivers and supported use cases  that you could try on the most recent Raspbian image from Raspberrypi.org. I know it's not ideal since it will kill a lot of time :-( ...

    I too will try it on the latest raspbian that I can download (I may as well exercise the RPI CPU while I do other stuff) to see if the instructions work ok on the latest image, and can paste the log of the steps I took, so you can repeat it. However I don't have a Wolfson Pi card to confirm that aspect of functionality.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago in reply to shabaz

    HI Shabaz,

     

    Here is the link http://downloads.element14.com/wolfson/wolfson_3.10_master.zip?COM=WolfsonAudioCard

    I will have a go on the method you suggested...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to saurocksall

    Hi Saurabh,

     

    Just to let you know, the process to compile the kernel natively on the RPI will take an extremely long time. I started last night, and 12 hours later it is still building. This is without any overclocking or other parameter changes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • saurocksall
    saurocksall over 12 years ago in reply to shabaz

    Hi Shabaz,

     

    Thanks for your efforts, I really appreciate them. I am not a software guy so it is really tough thing for me, have you checked out ragnar.jensen's image file ??