Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Wolfson Audio Card for Raspberry
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bharatrai888
  • Date Created: 29 Mar 2014 3:43 PM Date Created
  • Views 979 views
  • Likes 0 likes
  • Comments 1 comment
  • raspi
  • raspberrypi
  • rocking_pi
Related
Recommended

Wolfson Audio Card for Raspberry

bharatrai888
bharatrai888
29 Mar 2014

Hey Friend,


This week I got a mail from element14 that they are providing Wolfson Audio module to the participants. I haven’t received the product yet may be courier service to my area is poor.


Talking about the Wolfson Audio Card it has various features as follow


  • Audio hub CODEC with integrated voice processor DSP
  • Programmable audio effects and voice processing functions
    • Transmit-path noise reduction and echo cancellation
    • Receive-path enhancement and noise reduction
    • Wind noise, sidetone and other programmable filters
    • Dynamic Range Control, Fully parametric EQs
  • Multi-channel asynchronous sample rate conversion
  • Integrated 6/7 channel 24-bit hi-fi audio hub CODEC
    • 6 ADCs, 96dB SNR microphone input (48kHz)
    • 7 DACs, 113dB SNR headphone playback (48kHz)
  • Audio inputs
    • Up to 6 analogue or digital microphone inputs
    • Single-ended or differential mic/line inputs
  • Multi-purpose headphone / earpiece / line output drivers
    • 2 stereo output paths
    • 29mW into 32Ω load at 0.1% THD+N
    • 100mW into 32Ω BTL load at 5% THD+N
    • 6.5mW typical headphone playback power consumption
    • Pop suppression functions
    • 2.3μVRMS noise floor (A-weighted)
  • Mono BTL earpiece output driver
  • 2 x 2W stereo Class D speaker output drivers
    • Direct drive of external haptics vibe actuators
  • Two-channel digital speaker (PDM) interface
  • SLIMbusRegistered audio and control interface
  • 3 full digital audio interfaces
    • Standard sample rates from 4kHz up to 192kHz
    • Ultrasonic accessory function support
    • TDM support on all AIFs
    • 8 channel input and output on AIF1
  • Flexible clocking, derived from MCLKn, BCLKn or SLIMbus
  • 2 low-power FLLs support reference clocks down to 32kHz
  • Advanced accessory detection functions
    • Low-power standby mode and configurable wake-up
  • Configurable functions on 5 GPIO pins
  • Integrated LDO regulators and charge pumps
  • Support for single 1.8V supply operation
  • Small W-CSP package, 0.4mm pitch

 

Applications

 

  • Smartphones and Multimedia handsets
  • Tablets and Mobile Internet Devices (MID)
  • General-purpose low-power audio CODEC hub

 

 

If talking about its use in our project as earlier I am using RaspBMC for implementation of Karaoke on raspberry pi. Unluckily searching on internet I found that for now it can only works on new built of raspbian. I am not sure how much it is correct. So I have to check once it arrives If it works it is good news if not then I will have to search for some different ways to implement karaoke which utilizes the new wolfson audio card

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    HI,

     

    Can you email regarding @ lslater@newark.com

     

    With Thanks,

    L.Slater