Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Blog BEEhavior Investigation
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: msimon
  • Date Created: 19 Jan 2023 1:47 PM Date Created
  • Views 1531 views
  • Likes 10 likes
  • Comments 9 comments
  • save the bees
  • BEEhavior
Related
Recommended

BEEhavior Investigation

msimon
msimon
19 Jan 2023

Unfortunately, like many of you, I do not have access to a bee hives. I have no prior knowledge of bee care and have relied on information found through internet research. I thought it will be a good start to share my initial idea discuss it until we have the boards to have hands on experiment. 

Here are some of the ideas I have found.

The weight of the hive can be useful. If bees are producing honey in the season, the weight is expected to rise. However, if the weight is decreasing unexpectedly, it is a warning that bees may need some food or the colony is losing its members.

Temperature should be conserved inside the hive. ChatGPT answer this question like "The ideal temperature for a hive is between 95-100°F (35-38°C). This temperature range allows the bees to easily move around the hive and properly care for the brood. If the temperature inside the hive drops below this range, the bees may struggle to keep the brood warm and healthy. On the other hand, if the temperature inside the hive becomes too hot, the bees may become stressed and less productive."

Similarly, humidity also should be at certain range around 40-60%. If humidity is too high, there may be problems like mold. It is also indicator that there are lots of dead bees inside the hive(Physics for beekeepers: mold in a beehive).

As temperature, humidity, and weight are crucial factors for the well-being of a bee colony, my initial task is to install sensors to measure these parameters both inside and outside the hive. Hopefully, this data provides valuable insights about what is happening in the hive. My initial idea is establish threshold values for the minimum and maximum temperature, humidity, and weight, as well as for the difference between the values measured inside and outside the hive. The speed of change and its direction is also need to be investigated. If there are multiple hives, comparing them also can be informative too. As I learn more insights about bees, I can modify the system. 

I also plan to include some audio processing. Still don't have what I am gonna do but after completing the sensory part, I will dedicate time for that. The sound provides number of bees, situation of the  pupal stage, and information about the queen (Acoustic Analysis of Bee Behavior). My initial thought is doing frequency analysis as it sounds easy at first stage.

The final stage can be about communication. This actually depends on where hive(s) is/are located. If you have only one hive in your garden, a Wi-Fi or cabled connection works. But if you have distributed hives in a rural area then you may need to think other RF communications protocols like LoRa.  

It looks like building the system will not be as difficult as signal processing and make inference from the data. I need to learn more about the bees so the plan may change on the go. If you have any suggestion feel free to share.

  • Sign in to reply
Parents
  • ralphjy
    ralphjy over 3 years ago

    Good start.  I'm researching what species of bee that I want to target.  It looks like you've decided on honey bees.

    There is some debate about introducing non-native species, so I'm going to contact local beekeeping organizations in my area.

    For the challenge there won't be time to get real data, but I'd like to use the opportunity to do something that will enhance the pollination in my neighborhood in the future and I don't want to accidentally do any harm.

    It looks like the finisher prize for the contest is appropriate for species like mason bees.  I noticed that is what the local community college garden uses.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to ralphjy

    I would imagine that the honeybee is pretty well looked after by beekeepers and probably easier to study if you have access to hives?

    The wild bees however appear to be important for a wider range of pollination, including crops, but are in steady decline so perhaps need more help? They are more popular in gardens so perhaps more accessible for citizen science?

    I guess it depends if you have a preference for jam or for honey on your toast at breakfast. Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 3 years ago in reply to ralphjy

    I would imagine that the honeybee is pretty well looked after by beekeepers and probably easier to study if you have access to hives?

    The wild bees however appear to be important for a wider range of pollination, including crops, but are in steady decline so perhaps need more help? They are more popular in gardens so perhaps more accessible for citizen science?

    I guess it depends if you have a preference for jam or for honey on your toast at breakfast. Slight smile