Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Blog ZinnBee Blog#03: LoRa WAN Communication Framework
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: flyingbean
  • Date Created: 12 Mar 2023 9:14 PM Date Created
  • Views 877 views
  • Likes 8 likes
  • Comments 0 comments
  • save the bees
  • nicla vision
  • lora
  • mkr1310
  • arduino
Related
Recommended

ZinnBee Blog#03: LoRa WAN Communication Framework

flyingbean
flyingbean
12 Mar 2023

It is time to be back on ZinnBee path at Element14 community after a while.  I am new for LoRa WAN technology, so I planned to finish the LoRa WAN framework before I jump into ML for Nicla Vision subsystem. Elment14 Community did great jobs on LoRa WAN projects.  I read a lot of them before I kicked off ZinnBee LoRa WAN communication framework.

I have been using two MKR1300s for initial LoRa WAN mock-up testing since last month because MKR1300 and MKR1310 are almost identical on LoRa WAN interface for the testing.  MKR1310 will be used until Nicla Vision subsystem is installed. I do not want to burn MKR1310 out by accident. Lessons were learned from my own history.

Part 01: LoRa WAN transmitter

I accidentally acquired a MKR IoT Carrier module last month from our local MicroCenter shop. It is a very beautiful carrier module, which is used for LoRa WAN transmitter base board in ZinnBee project. MKR1300 mounted on IoT carrier.

image

Fig 1. Arduino IoT Carrier Pin Map

MKR IoT carrier has a HTS221 sensor to measure humidity & temperature as Ref[1] described. HTS221 sensor will monitor the temperature around BEE environment.  

Here is the bench setup of LoRa WAN transmitter:

image

Fig 2: LoRa WAN IoT Carrier Transmitter

Part 02: LoRa WAN receiver  

The initial mock-up receiver is another MKR 1300 for the LoRa WAN framework. The receiver has a SD card logger, an OLED display and a RTC to track the real time. I selected official Arduino X000016 antenna for this project since I might not have enough time to test other 3rd party antennas on MKR1300/1310 platform (original deadline for ZinnBee project was March 17th, 2023). Arduino X000016 is a beautiful piece of part for bench testing, but the structure of the antenna might need extra work for the mounting project on my 3D design later.

Here is the  LoRa WAN  receiver schematics:

image

Fig 3: ZinnBee LoRa WAN Receiver Schematics

The breadboard circuit of ZinnBee LoRa WAN receiver is presented at Fig 4.

image

Fig 4: ZinnBee  LoRa WAN Receiver

Part 03: Bench Testing Report

The software code of LoRa WAN IoT transmitter was integrated from Arduino_MKRIoTCarrier example source codes and LoRa example code as Fig 5 and Fig 6:

image

Fig 5: Arduino_MKRIoTCarrier Examples

image

Fig 6: Arduino LoRa Examples

The final source code of the transmitter side code can be found from the link as below:

https://github.com/EE4fun/ZinnBee/blob/master/LoRa_WAN_Mockup/ZinnBee_LoRa_WAN_Sender_IoTCarrier.ino

The LoRa receiver side software source codes include 4 sections:

  1. LoRa receiver
  2. DS3231 (from eBay)
  3. SSD 1306 OLED display (0.96 inch OLED, White, from eBay)
  4. MicroSD adaptor card(3rd party part)

The baseline software codes for each building block can be found from links as below:

  1. LoRa receiver: LoRa example(Arduino LoRa library) à LoRaReiver
  2. DS3231 : https://mytectutor.com/ds3231-rtc-with-arduino-including-digital-clock-using-oled-display/
  3. SSD 1306 OLED : https://miliohm.com/how-to-draw-or-print-bitmap-to-oled-display-arduino/
  4. SD logger: Arduino SD library

The UART debugging messages from transmitter & receiver side are presented as Fig7.

IoT Carrier LoRa Transmitter                                   LoRa Receiver

image

Fig 7: ZinnBee LoRa WAN Framework Communication Messages

Where the temperature from IoT carrier board was measured at 71.92 F. The LoRa receiver side read the temperature from LoRa package as 71.92156 F. The RSSI  was -25, which means the LoRa WAN signal was pretty good on the bench testing. I will continue to check RSSI reading while I move the mock-up testing from indoor environment to outside next week. There are too much winter/spring storms in MN, US, now.

Here is the snapshot from OLED at the same moment as UART debugging messages shown in Fig 8.

image

 Fig 8: OLED Display Messages

Here is the snapshot of SD card logger:

image

Fig 9: SD Card Logs

Where most of the information were accurate enough, however, I did get one error character before °F. I need to debug it in the future blogs.

 The source codes of the mock-up testing are published at Github repo: https://github.com/EE4fun/ZinnBee/tree/master

 In order to promote the theme of the design challenge: Save The Bees, I made a logo with a Bee for OLED display splash:

image

Fig 10: ZinnBee Project Logo

I will start to work on ML/Edge Impulse tasks on Arduino Nicla on my next blog.

References:

Ref [1]   https://docs.arduino.cc/tutorials/mkr-iot-carrier/mkr-iot-carrier-01-technical-reference#humidity--temperature-sensor

ZinnBee Blogs as below:

 ZinnBee Blog#01: Introduction of the Project

ZinnBee Blog#02: Initial Project Structure