Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Knight Rider
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scrpn17w
  • Date Created: 21 Apr 2015 2:53 PM Date Created
  • Views 2106 views
  • Likes 3 likes
  • Comments 20 comments
  • kitt
  • knight_industries
  • knight_rider
  • sci_fi_your_pi
  • kitt_car
Related
Recommended

Knight Rider

scrpn17w
scrpn17w
21 Apr 2015

This is my build thread of turning my 1999 Honda Prelude into an emulation of KITT (Knight Industries Two Thousand) from the TV series "Knight Rider". There is going to be a lot of buttons, switches and various indicator lights. I'll add a small screen in the car for both interfacing with the Pi and displaying various data/Images/Videos. Then of course there are the 3 most recognizable traits of the car: The LED "scanner" on the front of the car, the unmistakable voice from the "AI" of the car, and the LED "visualizer" of the cars AI system. Being that I won't be able to make this quite as awe inspiring as the actual KITT and the car I'm using was made in 1999 I'm going to call it the K.I.N.N. (Knight Industries Nineteen Ninety-nine).

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 11 years ago +2
    Good Job! You might also wanna google "larson scanner" to cut down costs. I did that for my bicycle when I was a kid . A 555 and a 4017 can do wonders I tell ya. All the best! Cheers, IP
  • scrpn17w
    scrpn17w over 11 years ago +2
    After some Google image searching and not coming up with a suitable background to use for KITT's screen I decided to make my own. I found the highest quality "Knight Industries" logo that I could, re-sized…
  • scrpn17w
    scrpn17w over 11 years ago +2
    I did some digging around yesterday and came upon a project I started a few years ago. It started life as an old joystick for a windows 95 PC. I bought it as a yard sale for a couple dollars and immediately…
Parents
  • scrpn17w
    scrpn17w over 11 years ago

    image

    I went through the box of parts I received and got out most of the main components I'm going to use from it. I'm planning on using the Pi-2 as the central hub of the system, the Wi-Pi for wireless connections, the Chipkit-Pi to replace some of the Arduino modules and the Pi-Face board with relays on it to control high power draw items (oil slick pumps). I also decided to setup a breadboard/Arduino connection with a couple buttons and a thumb stick (variable Analog inputs) to start building up the control panel for the Pi. My plan for this week is to get the couple buttons and thumb stick working as an input to the Pi just so I have the basics down for getting the communication between the boards working. I'll add more buttons and switches later on. For now I'm starting small.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scrpn17w
    scrpn17w over 11 years ago

    image

    I went through the box of parts I received and got out most of the main components I'm going to use from it. I'm planning on using the Pi-2 as the central hub of the system, the Wi-Pi for wireless connections, the Chipkit-Pi to replace some of the Arduino modules and the Pi-Face board with relays on it to control high power draw items (oil slick pumps). I also decided to setup a breadboard/Arduino connection with a couple buttons and a thumb stick (variable Analog inputs) to start building up the control panel for the Pi. My plan for this week is to get the couple buttons and thumb stick working as an input to the Pi just so I have the basics down for getting the communication between the boards working. I'll add more buttons and switches later on. For now I'm starting small.