Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech: User Interface, optimization and simplification
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 16 Aug 2015 1:14 PM Date Created
  • Views 1575 views
  • Likes 2 likes
  • Comments 4 comments
  • interface_design
  • meditech_project
  • inter_process
  • python
  • user_interface
  • software_simplification
  • raspberry-pi
  • task_architecture
  • sci_fi_your_pi
  • multi_process
Related
Recommended

Meditech: User Interface, optimization and simplification

balearicdynamics
balearicdynamics
16 Aug 2015

Introduction

One way to optimize the behavior of the Meditech system is adopting the more reliable tools, programming languages and technologies depending on the different tasks that should be accomplished. This implies obviously a multi-language  environment, essential to reach the better simplification level; for example, following this primary directive, all where it is possible the MySQL database will be accessed via low level SQL queries with bash scripting techniques as well as the hardware control software is developed in gcc++.

 

This approach maybe a bit more complex than the choice of a unified development language, possibly at high level. In fact we should include in the pros of this fragmented approach also a better costs optimization involving hardware solutions just when it is not possible to solve them with software.

 

In the initial Meditech design one of the development platforms included in the project was Qt but then this directive changed, as Python revealed the better language to develop the main scripting sources controlling the Meditech sub-processes and a good way for the User Interface design, with some more extra effort.

 

Based on these considerations at the actual date the Meditech development scheme has totally excluded the Qt environment replaced by Python beside to the Linux scripting tools, SQL language, PHP and few other development components and libraries.

 

Involved software components

In the scenario described above every different software environment adopted in the system should be viewed as a set of one ore more specialized package(s) set. The following diagram shows the general scheme.

image

First of all this methodology tend to take the maximum advantage working in a multi-task environment. As it has been already discussed in the previous posts, Meditech is a modular system using an internal set of three specialized Raspberry PI devices, plus a fourth unit dedicated to the camera features but other can be added if needed. The same described vertical task approach has been adopted in all the devices as the software model.

In the scheme we identify different classes of applications, harmonized and integrated by an inter-process controller developed in python.

 

The software sections in detail

 

On-demand processes

These are processes that most include the network connection (e.g. launching a task on another unit of the system); are bash scripts that launch a task execution when the behavior needs it. A typical example is the process TTS (Text-To-Speech) playing a synthesized sentence in response to a command. The task-on-demand can be called by other processes or by the main inter-process controller; they have the characteristic that we should always expect and exit condition.

 

Background processes

This group includes that startup Linux services, like the peripheral controls, Apache2 web server, the Php engine etc. Then there are Meditech-specific processes that starts when the device is powered-on and runs indefinitely. A typical example is the infrared controller running over the lirc ervice (Linux Infrared Controller) managing the Infrared controller interface, the primary interaction method with the system.

 

Networking

Beside the OS networking services, including but not only the SSh server, web server, MySQL server, NTP server and more, there are other Meditech-specific networking services based on bash scripting commands to manage some special network features like the remote database update, image streaming, continuous data processing intra-networking data exchange etc.

 

Database storage

This the class of tasks related to the local MySQL database management and the remote server update (when there is an active Internet connection). Where the SQL queries are recursive tasks these are embedded in bash scripts (to simplify the calls) while in the interactive UI the database is used as data collector and the information retrieved from the sensors are represented graphically on the screen widgets with Python and PythosnSQL programs.

 

Hardware control

The control panel and the data acquisition from the probes is developed under GCC commands that are embedded in bash scripts.

 

User Interface and interactivity

The Meditech UI is developed in Python and the visualization of the various widgets is controlled by the inter-process control developed in Python too.

 

Internet web access

This class of tasks is divided in a double client-server mechanism to enable the remote support from any authorized remote Internet connection (it is sufficient a browser). on the Meditech side the Apache2 + MySQL and PHP engine grant the remote access from the same LAN. Using a could server when an Internet connection is active and the remote assistance support has been enabled by the local operator the data are sent real-time over a cloud MySQL server. A PHP-based web site grant the accessibility from remote to the data and enable the chat support with the local Meditech device.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Good post and description of the various levels of control. DAB
Parents
  • jw0752
    jw0752 over 11 years ago

    I enjoyed reading your post. Would this approach present any problems if the unit was commercialized and had to be serviced by someone other than you?

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to jw0752

    This post is a sort of introduction, then it will be followed by other two pointing the attention on the task controller and the python user interface; probably some things will be more clear then.

     

    No problem servicing the product: this is one of the most important reasons that I have done it modular. All the hardware components will be pre-loaded and the single part is reasonable cheaper so it is the worth to replace it instead of trying to repair. The linux version that will be installed in the Meditech devices is a custom version of the standard distribution so it should be plug-and-play.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to jw0752

    This post is a sort of introduction, then it will be followed by other two pointing the attention on the task controller and the python user interface; probably some things will be more clear then.

     

    No problem servicing the product: this is one of the most important reasons that I have done it modular. All the hardware components will be pre-loaded and the single part is reasonable cheaper so it is the worth to replace it instead of trying to repair. The linux version that will be installed in the Meditech devices is a custom version of the standard distribution so it should be plug-and-play.