Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog TrainingSphere - 12 - Blob detection
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: amgalbu
  • Date Created: 24 Sep 2015 8:09 AM Date Created
  • Views 872 views
  • Likes 1 like
  • Comments 0 comments
  • opencv
  • sci_fi_your_pi
  • cvblob
  • training_sphere
Related
Recommended

TrainingSphere - 12 - Blob detection

amgalbu
amgalbu
24 Sep 2015

In this post we will face some image processing technique, like blob analysys.

I will use the cvBlob library to detect blobs in the image capture by the raspicam

 

Step1: cvBlob installation

1.       Download cvBlob library from this link

               https://github.com/Steelskin/cvblob              

          and save it to

          /home/pi/cvblob

2.       Because I downloaded the zip file, I need to unzip it

               tar xvf cvblob-0.10.4-src.zip

3.       We need to make some bug fixing. So move to the source code directory

cd cvblob

cv cvBlob

and make the following  changes to

               a.       cvblob.h: at line 84 replace

const char cvChainCodeMoves[8][2] = { {0, -1},

with

const signed char cvChainCodeMoves[8][2] = { {0, -1},

               b.      cvlabel.cpp: at line 34 replace

const char movesSE[4][3][4] = <line continues...>

with

const signed char movesSE[4][3][4] = <line continues...>

               c.       cvlabel.cpp: at line 40 replace

const char movesI[4][3][4] = <line continues...>

with

const signed char movesI[4][3][4] = <line continues...>

4.       build cvBlob library

                    cd ..    

          cmake .    

          make

5.       and finally let's install the cvBlob library

               make install


Step2: develop an application that can detect blobs in images

  1. I firstly created some utility functions to capture images from RaspiCam. You can find such functions in raspistill.h and raspistill.c (everything is under development, so some code clean up may be required..). Thanks to raspistill functions, the main application is very easy to implement:

raspistill_initialize(&state);     
raspistill_shot(&state, camera_callback);     
raspistill_terminate(&state);              

The raspistill_shot take a photo and invoke the camera_callback function. The only      parameter used by this function is an IplImage object that contains the captured image

2.       Next step is to implement functions for detecting blobs in the image. Such functions are implemented in the blobs.c and blobs.h functions. There are two functions currently implemented

detectBlobs(IplImage* image, struct ImageParams* imageParams)          

                  and        

detectBlobsWithImage(IplImage* image, struct ImageParams* imageParams)              

The second one shows the results of the image processing in a set of windows. So I'm going to use the latter for this demo because it's more impressive than some text output on a console. This function basically gets the images captured by the RaspiCam and creates an image (named segmentated) where the pixel whose color is inside the given RGB color range are white and the other pixels are black

IplImage* segmentated;
cvInRangeS(image, CV_RGB(155, 0, 0), CV_RGB(255, 130, 130), segmentated);






With the segmentated image, we can detect blobsIplImage* labelImg;CvBlobs blobs;

labelImg = cvCreateImage(cvGetSize(image), IPL_DEPTH_LABEL, 1);
 
result = cvLabel(segmentated, labelImg, blobs);

3.       Let's bring everything together and make  loop that periodically invoke the raspistill_shot function so that we can experiment with the camera and it's behavior in different light conditions

4.       Let's build application with the usual sequence of commands

                    cd build    

          cmake ..    

          make