Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog TrainingSphere - 2 - Action plan
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: amgalbu
  • Date Created: 28 Jun 2015 7:34 AM Date Created
  • Views 345 views
  • Likes 2 likes
  • Comments 3 comments
  • sci_fi_your_pi
  • training_sphere
  • sci_fi_pi
Related
Recommended

TrainingSphere - 2 - Action plan

amgalbu
amgalbu
28 Jun 2015

The TrainingSphere is basically a coax drone based on the Raspberry board.

There is a very interesting project (Navio+) that is a porting of the ArduPilot software on a Raspberry board. Navio+ software is supposed to be used with their own board, but this board is very expensive and have a lot of features I don't actually need for this project. So I will try to create an APM that uses a different set of sensors specifically designed for indoor use, namely

  1. position will be based on the recognition of a given landmark
  2. altitude will be provided by a sonar
  3. as accelerometer I will the MicroStack accelerometer provided with the challenge kit

 

Given these assumptions, the plan for building the TrainingSphere includes the following steps

  1. Install Realtime Wheezy
  2. Install OpenCV on Raspberry board
  3. Install Blob detection library
  4. Make a simple blob detection application
  5. Make an application that can measure distance from a landmark of known size
  6. Test the sonar sensor
  7. Modify the ArduPilot code to accept input from the new sensors
  8. Modify the motor control output to provide a PWM that varies from 0% to 100% (currently the motor control output is a PWM that is compatible with any servo input)
  9. Build the TrainingSphere frame
  10. Add laser pointer
  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 10 years ago in reply to tomaja +1
    Hi Dragan It's likely I will not complete it in the remaining timeframe, but UAVs are something I would have liked to have some experience on, and this is a good opportunity When I was younger I used to…
Parents
  • tomaja
    tomaja over 10 years ago

    Good plan, Ambrogio. This sounds like a VERY serious project!

    Do you have experience in making RC multirotors or airplanes?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • tomaja
    tomaja over 10 years ago

    Good plan, Ambrogio. This sounds like a VERY serious project!

    Do you have experience in making RC multirotors or airplanes?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • amgalbu
    amgalbu over 10 years ago in reply to tomaja

    Hi Dragan

    It's likely I will not complete it in the remaining timeframe, but UAVs are something I would have liked to have some experience on, and this is a good opportunity

    When I was younger I used to build RC airplanes, but I don't have any experience with autonomous flight

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 10 years ago in reply to amgalbu

    You should give it a try anyway. Even a manually controlled orb with Raspberry Pi would be interesting to see. I will follow your progress for sure.

    Good luck!

     

    Dragan