It's time to start doing something serious!
So, according to the plan, I will install the realtime version of the Raspbian. I will use Raspberry Pi Model B. I will install this Raspbian version with real-time kernel for Raspberry Pi 2 Model B. It is based on 2015-02-16-raspbian-wheezy with default kernel replaced to 3.18.9-rt5-v7+ kernel and a few additional tunings.
Default Raspbian kernel 3.18 is configured with PREEMPT option and provides worst case latency around hundreds of microseconds. Real-time demanding applications require lower latencies than that. Real-time patch lowers the worst case latency to tens of microseconds, improving performance of real-time applications such as autopilots to be run on Linux.
Emlid (the company that provides this Raspbian version) provides also some useful performance comparisons
By the way, the following interrupt latency data (obtained by running command)
sudo cyclictest -l1000000 -m -n -a0 -t1 -p99 -i400 -h400 -qgives another idea of the performance improvements between Raspberry Pi and Raspberry Pi 2
Interrupt Latency | Raspberry Pi | Raspberry Pi 2 | ||
No RT | RT | No RT | RT | |
Min | 13 us | 11 us | 13 us | 11 us |
Avg | 23 us | 23 us | 21 us | 18 us |
Max | 1153 us | 66 us | 307 us | 58 us |
The step to install the realtime Raspbian are
- download image from
http://docs.emlid.com/Downloads/Real-time-Linux-RPi2/ - unzip the .xs file using 7-Zip. This will create a .img file
- dump the image on a SD card using Win32DiskImager
Very smooth and easy!

Top Comments
-
e14 Contributor
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
clem57
in reply to e14 Contributor
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
-
e14 Contributor
in reply to clem57
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
e14 Contributor
in reply to clem57
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children