Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog TrainingSphere - 5 - Building APM
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: amgalbu
  • Date Created: 9 Jul 2015 3:31 PM Date Created
  • Views 511 views
  • Likes 2 likes
  • Comments 1 comment
  • apm
  • raspberry-pi
  • sci_fi_your_pi
  • training_sphere
Related
Recommended

TrainingSphere - 5 - Building APM

amgalbu
amgalbu
9 Jul 2015

Building APM


Since I expect I will have to make some changes to the code, I will now try to build APM fro source code. Working repository for Navio APM port is on GitHub.

I decided to build APM directly on your Raspberry Pi since it does not require to setup a cross-compiling environment and Raspberry Pi has enough computing power to make this step fast enough


Download the APM’s port for Navio:


git clone https://github.com/emlid/ardupilot.git


Switch to the 'navio' branch:

git checkout navio


Navigate to the autopilot’s directory, for example rover, run configuration and build it:

cd ardupilot/ArduCopter
make configure
make navio-heli


I'm not sure the heli configuration fits my needs, but I will try a build with this configuration, then I will change the makefile. Many other frames are supported. To build for other frame types replace heli with one of the following options:

quad tri hexa y6 octa octa-quad heli single obc nologging

 

Executable file will be placed in /tmp/APMcopter.build directory. Copy the binary from tmp directory to your home folder:

cp /tmp/APMcopter.build/APMcopter.elf /home/pi/APMcopter.elf

 

Running APM

To run APM use the following (change APMrover2.elf to ArduCopter.elf or ArduPlane.elf if needed):


sudo ./APMcopter.elf -A udp:192.168.1.2:14550


Where 192.168.1.2 is the IP address of the device with the Ground Control Station – your laptop, smartphone etc.

 

Arguments specify serial ports (TCP or UDP can be used instead of serial ports) :

  • -A is for telemetry
  • -B is for external GPS
  • -C is for secondary telemetry

If you would like to transfer secondary telemetry over the UART port on Navio you can specify it like this:

 

sudo ./APMcopter.elf -A udp:192.168.1.2:14550 -C /dev/ttyAMA0

Autostarting APM on boot

To automatically start APM on boot add the following (change -A and -C options to suit your setup) to /etc/rc.local file on your Raspberry Pi:


sudo /home/pi/APMcopter.elf -A udp:192.168.1.2:14550 -C /dev/ttyAMA0 > /home/pi/startup_log &


  • Sign in to reply
  • balearicdynamics
    balearicdynamics over 11 years ago

    Hi Ambrogio,

     

    nice post, things start assuming always more consistence ... Do you plan to put somewhere on a repo also the customised versions of your packages?

     

    Enrico