Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Video conferencing with the Raspberry Pi part 2
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 9 May 2015 1:13 PM Date Created
  • Views 816 views
  • Likes 3 likes
  • Comments 2 comments
  • realife_holo
  • design_challenge
  • scifi_your_pi
  • reallife_holo
Related
Recommended

Video conferencing with the Raspberry Pi part 2

e14 Contributor
e14 Contributor
9 May 2015

After probably having broken my pi camera last week, I tried to revive it, but to no avail. At this point it's probably safe to call it a lost cause. I wasn't too worried over it. I have 2 USB webcams lying around and I figured I might be able to just use one of those instead instead.

In fact, these USB webcams have a built-in microphone. In absence of the Cirrus Logic audio card, that would really come in handy!

 

image

Meet Laurel and Hardy

 

The left one is a Microsoft LifeCam VX-3000, the right one is an MSI StarCam 370i. They might look like a wacky duo but both have served me well and are fully functional webcams. That being said, I can't seem to make them work on the Pi.

They are both correctly detected when I connect them.

Here's dmesg and lsusb for the MSI camera:

 

[  252.049044] usb 1-1.2: new full-speed USB device number 6 using dwc_otg

[  252.151553] usb 1-1.2: New USB device found, idVendor=0c45, idProduct=60fc

[  252.151579] usb 1-1.2: New USB device strings: Mfr=0, Product=1, SerialNumber=0

[  252.151597] usb 1-1.2: Product: USB camera

[  252.205066] gspca_main: v2.14.0 registered

[  252.211258] gspca_main: sonixj-2.14.0 probing 0c45:60fc

[  252.214266] input: sonixj as /devices/platform/bcm2708_usb/usb1/1-1/1-1.2/input/input2

[  252.215734] usbcore: registered new interface driver sonixj

[  252.302998] usbcore: registered new interface driver snd-usb-audio

pi@raspberrypi ~ $ lsusb

Bus 001 Device 006: ID 0c45:60fc Microdia PC Camera with Mic (SN9C105)


And Microsoft:

[  417.699011] usb 1-1.2: new full-speed USB device number 7 using dwc_otg

[  417.801644] usb 1-1.2: New USB device found, idVendor=045e, idProduct=00f5

[  417.801672] usb 1-1.2: New USB device strings: Mfr=0, Product=1, SerialNumber=0

[  417.801690] usb 1-1.2: Product: USB camera

[  417.803249] gspca_main: sonixj-2.14.0 probing 045e:00f5

[  417.806077] input: sonixj as /devices/platform/bcm2708_usb/usb1/1-1/1-1.2/input/input3

pi@raspberrypi ~ $ lsusb

Bus 001 Device 007: ID 045e:00f5 Microsoft Corp. LifeCam VX-3000

 

The drivers appear to be correctly loaded and Iceweasel shows that both the camera and the built-in microphone are available.

image

why yes, I would like that

 

As soon as I try to actually use either camera though, no video or audio comes through and I see hundreds of these errors in dmesg:

[12380.380712] gspca_main: ISOC data error: [8] len=0, status=-71

[12380.380721] gspca_main: ISOC data error: [9] len=0, status=-71

[12380.380730] gspca_main: ISOC data error: [10] len=0, status=-71

[12380.380738] gspca_main: ISOC data error: [11] len=0, status=-71

[12380.380747] gspca_main: ISOC data error: [12] len=0, status=-71

 

...and these:

[12452.042127] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

[12452.170150] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

[12452.298154] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

[12452.426173] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

[12452.554196] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

[12452.682204] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

[12452.810219] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

[12452.938235] sonixj 1-1.2:1.0: URB error -71, resubmittingsonixj 1-1.2:1.0: URB error -71, resubmitting

 

Searching the web for what that error -71 means lead me to this Debian bug report. The issue appears to be very generic and I don't think I could get any webcam to work on Raspbian right now. It's really too bad but for the time being I'm going to give up on getting a camera to work with the Raspberry Pi. image

  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago +1
    Just ask, and I'll get you a camera board. I know where you work
  • crimier
    crimier over 11 years ago

    Hi! It's really interesting seeing videoconferencing work on Linux, had always been curious about that =) I recommend you use a Logitech webcam, they're really handy and work with Linux without any problems. They also are well worth the price - I'd gotten 2 of these for 20EUR each and it's been a great investment so far. Image quality is good, microphone works better than laptop's integrated one, by the way, one of them also served as a surveillance camera, basically active 24/7 for about half a year on some OpenWRT router =)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago

    Just ask, and I'll get you a camera board. I know where you work image