Sci-Pi Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sci-Pi Design Challenge
  • More
  • Cancel
Sci-Pi Design Challenge
Blog ROEVES - A Raspberry PI Underwater ROV
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sci-Pi Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: feiticeir0
  • Date Created: 26 Apr 2023 12:35 PM Date Created
  • Views 2081 views
  • Likes 7 likes
  • Comments 6 comments
  • sci-pi
  • ROEVES
  • raspberry pi
  • rov
  • sci-pi design challenge
Related
Recommended

ROEVES - A Raspberry PI Underwater ROV

feiticeir0
feiticeir0
26 Apr 2023
ROEVES - A Raspberry PI Underwater ROV

image

Hi all ! Hope everyone is great.

My project will consist on building a Underwater ROV (Remote Operated Vehicle) , the cheapest way possible, using just off the shelf items.

What's a underwater rov ?

A remotely operated vehicle (ROV) is an unoccupied underwater robot that is connected to a ship (typically) by a series of cables. These cables transmit command and control signals between the operator and the ROV, allowing remote navigation of the vehicle. An ROV may include a video camera, lights, sonar systems, and an articulating arm. The articulating arm is used for retrieving small objects, cutting lines, or attaching lifting hooks to larger objects.

While there are many uses for ROVs, some of the most common hydrographic applications include object identification (for submerged navigation hazards) and vessel hull inspections. An ROV is not intended to be a replacement for hydrographic diver investigations, but could serve as a substitute if divers are not available or diver safety is in question.

(by NOAA)

Types of ROV

In the ROV world, they are seperated into size categories, which also corresponds with their capability. The terminology can vary, but generally, the following are used to define the range in size

Work Class

They are the size of a mini-bus and weigh a few thousand kilograms. They required a LARS (Launch and Recovery System) to deploy a highly skilled operators.

Light work class

These are smaller, that weigh a few hundred kilograms and are the size of a large quad bike. They still require a LARS, but can be deployed from smaller vessels.

Inspection (or Observation)

There are the size of a lounge chair and weigh around 100kg. Can be deployed from a smaller vessel. Although they can be deployed by a couple of operators, some still require a LARS.

Mini or micro class (portables)

These weigh less than 50kg and can be deployed and recovered by just one or two people. They are generally used for visual inspection.

(by Reach Robotics)

ROEVES

ROEVES will be a mini ROV, built around a Raspberry PI. It will have a camera, a camera v3 module because of the auto-focus functionality. It will have one or two LEDs to light up the way.

The forward/backward movement will be controlled by a motor on the bottom and two motors (one on each side) for up/down. The ROV will be tethered to the control command .

It will be streaming using the camera, with the possibility of recording.

With the help of my friend DALL-E, the ROV will be, roughly, like this:

ROEVES

In the end, we shall see. It lacks the motors and other details, but the overall shape is there. Slight smile

Possible problems

I'm expecting my biggest problem to be waterproofing and buoyancy .

A 3D printed object is not waterproof, but there are ways we can change that. Some tricks that can be used while printing and designing the object and there's some post-processing that can be done.

I'm going to make some testing to see what is better.

There are some projects out there that use a Pixhawk (a drone Flight Controller) to control the stability of the rov, but it costs upwards 150€ and that's just too expensive.  I'm going to try this without any of that. We will see how it behaves.

So, stay tuned and let the fun experience begin.

Cheers.

  • Sign in to reply
Parents
  • dougw
    dougw over 3 years ago

    Very cool design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 3 years ago

    Very cool design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • feiticeir0
    feiticeir0 over 3 years ago in reply to dougw

    The question will be - can I turn it in to a 3D design ? Smiley

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to feiticeir0

    You could 3D print a mould and then use fibreglass to create the waterproof hull. A bit like some boatbuilding.

    Either that or place the electronics inside a waterproof tube and then place that inside the 3D printed shell. Might get some ideas from this project:
    /challenges-projects/element14-presents/project-videos/w/documents/27861/episode-576-build-your-own-underwater-drone-with-3d-printed-parts