Shift it! Warehouse Automation Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Shift it! Warehouse Automation Design Challenge
  • More
  • Cancel
Shift it! Warehouse Automation Design Challenge
Forum Warehouse 13: V: Warehouse in motion
  • News
  • Forum
  • Projects
  • Leaderboard
  • Files
  • Members
  • Mentions
  • More
  • Cancel
  • New
Join Shift it! Warehouse Automation Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 44 subscribers
  • Views 813 views
  • Users 0 members are here
  • flight simulator
  • nexgen
  • Stack it
  • count
  • mysql
  • shift it
Related

Warehouse 13: V: Warehouse in motion

phoenixcomm
phoenixcomm over 2 years ago

image Ok, hears a quasi normal day here I get product for 2 or 3 sources, eBay, distribution (PO), stores, etc. When a PO is required I generate one. If not required, I just insert into history table as a purchase and tag it with a project, that could turn into a PO.
Now back here I get something from somewhere. Well first I have to check two tables the Manufactures and add if necessary, then get its Category's ID  with those .two pieces I can now generate the Info table, If it is in the table we just generate the History. But wait you say does this go into the warehouse?
Ok the parts are from eBay, and there for my simulator MCT275, a opto-isolator, and made by Vishay, and there are 200 of them. Well I have to start at the beginning. OK I check the Manufactures table and its not there so I add it. It has an ManID = 19. Now I check the Categories table and the CatID = 1377 (Integrated Circuit, Opto-isolators). Now I go to the Info table and put in all the data. I have left the CatSeq blank, as the computer will update the CatSeq number to one higher than in the Categories table if its Null then its a 1 and and we update the Info tables CatSeq number buy the  InfoID number of the part. This is done autonomously so CatSeq numbers are always correct. Next I need to add to the History table. Since I don't have an extra bin in my blue draws for them, I will keep them in their tubes, on the self where to two project boxes are. So lets see where they are. This requires a Spots its Location = Office, UnitID = C, ShelfID = 2 (above the lab bench), Spot = F, and here is its picture.
imageThere they are right where I had to put them.  --------->

If This had been a Purchase Order or eBay for that mater I would have had the Info table filled out before hand. So when I received the product all I would have done is fill in the History table. Note my system lacks one important feature. and that would be the Receiving and RecItems tables, I might add them later.

Now that there in the "Warehouse" how do I get them out, I need some sort of paper trail. that's where my History table comes in. So lets say I need 10 of the Opto-isolators, for project Master Caution System. What to do. Go into the table and fill in the information CatID, CatSeq, Condition Code, Quan, Invoice, Quan-Sold. For the Invoice we have to get creative. We fill-in "Pro-MSC" (Project Master Caution System) and for each item going into that project we need that invoice tag. The system will autonomously fill in dates, PriceLot, PriceEa from the purchase entry in the DB. The reason we have to get creative is because invoice number are yearmonthSequence. I could change the invoice to a number but then I cant find it. So to keep everything copacetic I would have to add a invoice number modifier, or a cross over table.

Questions?

  • Sign in to reply
  • Cancel
Parents
  • javagoza
    javagoza over 2 years ago

    It is difficult to have the discipline to carry out all this routine and bureaucratic task. The more I think about it, the clearer I see a solution for this using a conversational interface, a chatbot like Rasa or DialogFlow acting against Gemini, for example, to convert requests into instructions for the database. I am involved in another design challenge, Extreme Environments, I don't know if I will have time to participate in this one once the other one is finished and there is no other temptation involved.

    In any case, I find it very interesting how you approach and describe the problem, good work and good luck with your project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 2 years ago

    It is difficult to have the discipline to carry out all this routine and bureaucratic task. The more I think about it, the clearer I see a solution for this using a conversational interface, a chatbot like Rasa or DialogFlow acting against Gemini, for example, to convert requests into instructions for the database. I am involved in another design challenge, Extreme Environments, I don't know if I will have time to participate in this one once the other one is finished and there is no other temptation involved.

    In any case, I find it very interesting how you approach and describe the problem, good work and good luck with your project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to javagoza

     javagoza Nope it realy wouldn't work as you have to train it for every operator! besides a chatbot is for weak minds..  In my project smarthab.us to ask you if you want something to drink water (it will dispense it for you sorry no beer at this time  ~~ Cris 

    BTW all of it is mundane its labels are all barcoded and every thing must be entered correctly. That is why when we order something there is a PO involved. and cross-checked with receiving docs. BEFORE it goes to the warehouse!

    MBTW! touch screen monitors are a must!