Shift it! Warehouse Automation Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Shift it! Warehouse Automation Design Challenge
  • More
  • Cancel
Shift it! Warehouse Automation Design Challenge
Forum TE Connectivity Connectors and MKR wiifi 1010
  • News
  • Forum
  • Projects
  • Leaderboard
  • Files
  • Members
  • Mentions
  • More
  • Cancel
  • New
Join Shift it! Warehouse Automation Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 45 subscribers
  • Views 285 views
  • Users 0 members are here
Related

TE Connectivity Connectors and MKR wiifi 1010

fyaocn
fyaocn over 1 year ago

image

1 Brief

*** it design challenge required TE Connectivity Connectors to be used in project and controlled with MKR wifi 1010. 

Here are the parts to be used in my project, five different connectors as follows.

2 TE Connectivity Connectors

2.1  8 position TE Connectivity's AMP RITS connectors . This Max Current rating is 3 A with  Voltage rating of 32 V DC.

image

This is easy to used in REMOTE INPUT/ OUTPUT TERMINAL SYSTEM (RITS).   Just insert the wires and press the housing.

image

For detail, the chisel shaped contact can clamp the wire tightly

image

2.2 8-position DYNAMIC D1000 SLIM WIRE-TO-WIRE CONNECTORS

Max Current rating is 4.5A and Voltage rating of AC/DC 250V. This is more widely used.

Here is the socket and plug for interlock,

image

image

And these are connectors for above connector housing.

image

image

Here is the details for connectors, this guarantee best connections.

image

3 MKR wiifi 1010

The MKR WIFI 1010 includes SAMD21, 32-bit ARM Cortex-M0+ with the usual rich set of I/O interfaces, and low power Wi-Fi with a Cryptochip for secure communication using SHA-256 encryption. With Flash Memory of 256 KB and SRAM of 32 KB.

image

This is the development board easy to used and fast in development. That is good to try new applications.

4 Summary

It takes some time to receive and gather the parts. Glad to get them all in time for the project design.

  • Sign in to reply
  • Cancel

Top Replies

  • fyaocn
    fyaocn over 1 year ago +1
    Here is the detail for two housing, one for TAB and one for receipt
  • fyaocn
    fyaocn over 1 year ago

    Here is the detail for two housing, one for TAB and one for receipt

    imageimage