Shift it! Warehouse Automation Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Shift it! Warehouse Automation Design Challenge
  • More
  • Cancel
Shift it! Warehouse Automation Design Challenge
Forum RTD P1000 wire was picking noise and is giving unsuitable reading
  • News
  • Forum
  • Projects
  • Leaderboard
  • Files
  • Members
  • Mentions
  • More
  • Cancel
  • New
Join Shift it! Warehouse Automation Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 45 subscribers
  • Views 700 views
  • Users 0 members are here
  • design challenge
  • shift it
Related

RTD P1000 wire was picking noise and is giving unsuitable reading

manojroy123
manojroy123 over 1 year ago

RTD P1000 wire was picking noise and is giving unsuitable reading. How to filter those noise.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 1 year ago +3
    1: avoid noise: use a clean power source (a battery is usually very low noise) use a front-end that's designed for precision measurement, and fit for this purpose 2: filter noise find the…
  • kmikemoo
    kmikemoo over 1 year ago +2
    You can also just use a running average of a bunch of measurements. This "technique" can be useful if you are looking for a relative shift in temperature more so than an accurate temperature reading. The…
  • michaelkellett
    michaelkellett over 1 year ago in reply to manojroy123 +2
    You have difficulty with solving problems because you do not have a good scientific approach. First you must define the problem in a complete and an-ambiguous way. It is IMPOSSIBLE to solve an inadequately…
  • Jan Cumps
    Jan Cumps over 1 year ago

    1: avoid noise:

    • use a clean power source (a battery is usually very low noise)
    • use a front-end that's designed for precision measurement, and fit for this purpose

    2: filter noise

    • find the nature of the noise. Frequency, signal noise ratio, is it drift or noise?
    • it may be possible to filter out known noise with sampling / acquisition techniques, analogue and digital filtering...

    Overall advice: the front end has to be good, and the same for the ADC part. Everything between the sensor, and having its value in a variable in your µcontroller.
    Investigate RTD front-end designs from IC manufacturers. They have app notes.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 1 year ago

    You can also just use a running average of a bunch of measurements.  This "technique" can be useful if you are looking for a relative shift in temperature more so than an accurate temperature reading.  The noise is in both readings so the difference between two running average measurements should be reasonably accurate.

    Even if you are looking for a single reading, the average of the readings compared to a simple thermometer will reveal if there is an offset - that could be compensated for with a correction factor or if the temperature reading is close enough to be acceptable.  Remember, just because the microcontroller's analog to digital converter gives you a value with a bunch of decimal places, it doesn't mean that the value is accurate or precise.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago

    You don't give enough context.

    How are  you using the RTD - 2 wire, 3 wire or 4 wire connection.

    How are you conditioning and measuring the signal (description and schematics, maybe software explanation as well).

    What is the environment (thermal, electrical  etc) and how long are the cables.

    What noise level are you looking for in your system (in equivalent degrees K)

    Are there any cost constraints.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • manojroy123
    manojroy123 over 1 year ago in reply to michaelkellett

    RTD- 2 wire

    measurement - thermal.

    used moving average but still not reliable. looking for something better filter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to manojroy123

    You have difficulty with solving problems because you do not have a good scientific approach.

    First you must define the problem in a complete and an-ambiguous way.

    It is IMPOSSIBLE to solve an inadequately defined problem.

    I asked you several questions about your noise problem and you have not answered even one of them.

    I asked:

    How are you conditioning and measuring the signal (description and schematics, maybe software explanation as well).

    You replied:

    used moving average but still not reliable. looking for something better filter.

    But this is not an adequate description

    I was expecting something like:

    Buffering and amplifying the signal with (schematic with values) having a gain of  X and a bandwidth of (Y)

    Sampling with a  12 bit ADC (type specified here) at Z Hz.

    Then processed by moving average filter averaging over N samples.

    You also need to specify the noise that is causing you problems:

    The data is extracted from the filter every Mth sample and the peak to peak noise of the extracted filtered data is P samples.

    This is equivalent to K degrees.

    You will need to use a scope or similar instrument to measure the spectrum and amplitude of the noise at the input of the ADC.

    If you present your problem as I've outlined above I will be able to help you and happy to do so.

    If you won't make the effort then neither will I.

    MK