Shift it! Warehouse Automation Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Shift it! Warehouse Automation Design Challenge
  • More
  • Cancel
Shift it! Warehouse Automation Design Challenge
Forum System software for checking motor temperature and for giving appropriate sound indication
  • News
  • Forum
  • Projects
  • Leaderboard
  • Files
  • Members
  • Mentions
  • More
  • Cancel
  • New
Join Shift it! Warehouse Automation Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 44 subscribers
  • Views 2958 views
  • Users 0 members are here
  • design challenge
  • shift it
Related

System software for checking motor temperature and for giving appropriate sound indication

manojroy123
manojroy123 over 1 year ago

Flowchart for detecting motor temperature and giving sound indiction.

image

In the above flowchart you can see how the system software works. First it checks for motor temperature and gives proper indication about it. Bellow is the working video of the system.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Arduino code

First we read sensor value from ADC.

 // Read sensor value
         int newValue = analogRead(A1);

Than we filter those value using median filter. Median Filter function code is given bellow. There were many software filter available like SMA(Simple mean average), LMA(Logarithmic mean average), median filter. SMA was still giving lots of error, so we have used median filter for processing sensor data. it was still giving some error. We are looking for more better software filter for processing sensor values.

/*Median Filter */
// Median filter function
int median(int *array, int size) {
  int sorted[size];
  // Copy array
  for (int i = 0; i < size; i++) {
    sorted[i] = array[i];
  }

  // Simple bubble sort
  for (int i = 0; i < size - 1; i++) {
    for (int j = 0; j < size - i - 1; j++) {
      if (sorted[j] > sorted[j + 1]) {
        int temp = sorted[j];
        sorted[j] = sorted[j + 1];
        sorted[j + 1] = temp;
      }
    }
  }
  

After filtering the Raw ADC sensor data using median filter. We convert the filtered value to voltage. Code for which is given bellow.

 int rawValue = filteredValue;
  float voltage = rawValue * 0.00323 ;  // Convert to voltage
  const float Rref = 992.0; //1K ohm referance resistor
 
  // Calculate sensor resistance from voltage divider formula
  float Rt =  Rref*( voltage / (3.307 - voltage));

After converting to voltage. We convert the voltage value to temperature using "Invert Callendar-Van Dusen" technique which has some constant in it. bellow is the code for it.

// Callendar-Van Dusen coefficients for standard PT1000 (α = 0.00385)
const float A = 3.9083e-3;
const float B = -5.775e-7; 
const float R0 = 1000.0;  // PT1000 resistance at 0°C

//Function for voltage to temperature convertion
float calculateTemperature(float Rt) {
  float temp = -A + sqrt(A * A - 4 * B * (1 - Rt / R0));
  temp = temp / (2 * B);
  return temp;
}

After doing all the required processes we simply print this value in serial terminal and give appropriate buzzer indication based on algorithm shown in flowchart. bellow is the code for it.

// the loop function runs over and over again forever
void loop() {
    digitalWrite(LED_BUILTIN, HIGH);
       delay(10);
      /*Median Filter Local Varibales*/
      // Read sensor value
         int newValue = analogRead(A1);
         int filteredValue;
      // Store new value in buffer
          readings[index1] = newValue;
          index1 = (index1 + 1) % windowSize;

      // Check if buffer is full
          if (index1 == 0) bufferFilled = true;


      // Apply median filter only when buffer is filled
  if (bufferFilled) {
    filteredValue = median(readings, windowSize);
    Serial.print("Raw: ");
    Serial.print(newValue);
    Serial.print("  Filtered: ");
    Serial.println(filteredValue);
  } else {
    Serial.print("Raw: ");
    Serial.print(newValue);
    Serial.println("  (Warming up)");
  }
         
       //Serial Read Write
     
       int rawValue = filteredValue;
  float voltage = rawValue * 0.00323 ;  // Convert to voltage
  const float Rref = 992.0; //1K ohm referance resistor
  float Res = (Rref*voltage)/(3.3-voltage);
 



// Calculate sensor resistance from voltage divider formula
  float Rt =  Rref*( voltage / (3.307 - voltage));

  // Invert Callendar-Van Dusen to get temperature (for T ≥ 0°C)
  float temp = calculateTemperature(Rt-20.0);

  Serial.print("Raw ADC Value: ");
  Serial.print(rawValue);
  Serial.print(" => Voltage: ");
  Serial.print(voltage, 3);  // 3 decimal places
  Serial.println(" V");
  Serial.println(" Resistance");
  Serial.println(Rt-20.0);
  Serial.println(" Temperature");
  Serial.println(temp);

//Buzzer program
  if(Rt > 1174 and Rt < 1194){
        digitalWrite(LED_BUILTIN, HIGH);   // turn the LED on (HIGH is the voltage level)
         delay(100);                       // wait for a 100 milisecond
           for(int a = 0; a<5; a++){
                            digitalWrite(LED_BUILTIN, LOW);    // turn the LED off by making the voltage LOW
                            delay(100);
                            digitalWrite(LED_BUILTIN, HIGH);   // turn the LED on (HIGH is the voltage level)
                            delay(100);  
                            }
        }
   else if(Rt >= 1194){
                         digitalWrite(LED_BUILTIN, LOW);   // turn the LED off (Low is the voltage level)
                         delay(1000);      
                      }
    

}

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 1 year ago in reply to manojroy123 +2
    Your code does not do that: if(Rt > 1174 and Rt < 1194){ // ... 48, 49 } else if(Rt > 1194){ // 51, 52... } 50° is unsafe according to your comment above (it's above 45°, but not above 50°). But…
  • Jan Cumps
    Jan Cumps over 1 year ago +1
    delay(100); // wait for a second This will not do what you expect. See the delay() documentation: Description Pauses the program for the amount of time (in milliseconds) specified as parameter…
  • michaelkellett
    michaelkellett over 1 year ago in reply to manojroy123 +1
    I have told you, in another thread, that you can't decide on a better filter without looking at the noise signals you want to get rid of and comparing them with the signal you want to keep. From what…
Parents
  • manojroy123
    manojroy123 over 1 year ago

    Does anyone knows any better software filter for sensor. Median filter still picks noise and displays it. But the probability of it is very low. lower than simple mean average filter. Any suggestions would be appriciated.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to manojroy123

    If you can't get a more stable measurement, you may have to make the median sample larger.

    How much do the measurements differ from what you think the temperature of the motor is? 1%, 10%, 100%, > 100% ?
    And are the measurements scattered around the expected value? 
    Maybe write a few 1000 measurements to a file, and draw a graph based on it. With a line showing what the expected measurement is?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • manojroy123
    manojroy123 over 1 year ago in reply to Jan Cumps

    After every 3 or 4 hour I get a beep even though temperature is 30'c. Beep for 45'c to 50'c and beep for 50'c 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • manojroy123
    manojroy123 over 1 year ago in reply to Jan Cumps

    After every 3 or 4 hour I get a beep even though temperature is 30'c. Beep for 45'c to 50'c and beep for 50'c 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to manojroy123

    Michael asked you earlier to read the questions, and give an answer that's related to the question.
    I think that advice would help here too. Your answer does not address the question.