Sixth Sense Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sixth Sense Design Challenge
  • More
  • Cancel
Sixth Sense Design Challenge
Blog Introduction to SensorTile Connection with Mobile App
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
  • Author Author: karthickiot
  • Date Created: 2 Mar 2019 4:19 AM Date Created
  • Views 1027 views
  • Likes 5 likes
  • Comments 1 comment
  • mobile app
  • sensortile
Related
Recommended

Introduction to SensorTile Connection with Mobile App

karthickiot
karthickiot
2 Mar 2019

Introduction:

The SensorTile is a tiny, square-shaped IoT module that packs powerful processing capabilities leveraging an 80 MHz STM32L476JGY microcontroller and Bluetooth low energy connectivity based on BlueNRG-MS network processor as well as a wide spectrum of motion and environmental MEMS sensors, including a digital microphone. It is complemented with software, firmware libraries and tools, including a dedicated mobile App.

  • Included in the development kit package:
    • SensorTile module (STEVAL-STLCS01V1) with STM32L476JG, LSM6DSM, LSM303AGR, LPS22HB, MP34DT05-A, BlueNRG-MS, BALF-NRG-02D3 and LD39115J18R
    • SensorTile expansion Cradle board equipped with audio DAC, USB port, STM32 Nucleo, Arduino UNO R3 and SWD connector
    • SensorTile Cradle with battery charger, humidity and temperature sensor, SD memory card slot, USB port and breakaway SWD connector
    • 100 mAh Li-Ion battery
    • Plastic box
    • SWD programming cable

 

SensorTile Front view SensorTile Back Viewimageimage

 

More details on Hardware and Software can be found in the following URL: https://www.st.com/en/evaluation-tools/steval-stlkt01v1.html

 

  • Software libraries and tools
    • STSW-STLKT01: SensorTile firmware package that supports sensors raw data streaming via USB, data logging on SDCard, audio acquisition and audio streaming.
    • FP-SNS-ALLMEMS1 and FP-SNS-MOTENV1: STM32Cube function packs
    • BlueMS: iOS and Android demo Apps
    • BlueST-SDK: iOS and Android Software Development Kit

 

The app is installed in the Android Phone, open it to connect the selected device.
imageimageimage

 

 

The sensor dashboard will display the sensor reading as in the below figures, the data can be store in SDcard or transfer to the remote device by cloud. Tab on the start logging to start the data recording like environmental and acceleration events.

 

imageimageimage

  • Sign in to reply
  • 14rhb
    14rhb over 7 years ago

    Great to see the data being sent from SensorTile to email.

     

    Do you have plans for using the STM32F411RE-Nucleo with this BLE capability. After flashing up the demo and Android App I could get the BLE to work but was unsure how that functionality could be brought back to the Nucleo board (which is where the rest of my robot code will be running). I guess the BLE data could be sent from the SensorTile to a modified Android App, used and sent BLE data back to the SensorTile. Also requiring the SensorTile code to be modified to receive that bespoke BLE data ?

     

    Rod