Sixth Sense Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sixth Sense Design Challenge
  • More
  • Cancel
Sixth Sense Design Challenge
Blog running with MCU controlled motor driver - Automatic Weeding Robot #8
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
  • Author Author: weiwei2
  • Date Created: 9 Mar 2019 3:46 AM Date Created
  • Views 1044 views
  • Likes 10 likes
  • Comments 3 comments
  • pwm pins
  • arduino ide
  • arduino ide to mbed
  • motor control applications
Related
Recommended

running with MCU controlled motor driver - Automatic Weeding Robot #8

weiwei2
weiwei2
9 Mar 2019

As i was testing nucleo64 in mbed notice that some arduino pin convention needs to be changed

for example, the pinMode in arduino need to be updated

pinMode(_pin1, OUTPUT)  ---> reconfigured as DigitalOut

i am wondering if there is any tutorial documentation that shows how to do conversion to MBED, listing every compatible command in arduino ide to what we have in MBED

 

Nonetheless, few days ago i tested with a MCU that uses the arduino IDE instead. Each of motor driver can be driven by a PWM pin and a directional pin. No grove shield is needed and this will save me one board

i want to verify that moving on grass has been resolved properly

 

My kid uploaded it at http://vt.tiktok.com/JLFovA/

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

so at least for sure now it is capable of running on its own on grass

 

to make it run, the arduino code is pretty simple

first put in the header file and define the pin in arduino ide style

 

#include "CytronMotorDriver.h"

// Configure the motor driver.
CytronMD motor1(PWM_DIR, 3, 4);   // PWM 1A = Pin 3, DIR=4 
CytronMD motor2(PWM_DIR, 5, 7); // PWM 2A = Pin 5, DIR=pin 7

 

then, define the moving command, here moving forward is shown

 

void movefront()
{
  motor1.setSpeed(128);   // Motor 1 runs forward at 50% speed.
  motor2.setSpeed(128);  // Motor 2 runs forward at 50% speed.
  delay(1000);
  
  motor1.setSpeed(255);   // Motor 1 runs forward at full speed.
  motor2.setSpeed(255);  // Motor 2 runs forward at full speed.
  delay(10000);


  motor1.setSpeed(0);     // Motor 1 stops.
  motor2.setSpeed(0);     // Motor 2 stops.
  delay(5000);  
}

 

then we can just call it move forward or backward, example

// The loop routine runs over and over again forever.
void loop() {
movefront();
delay(2000);
movefront();
delay(2000);
moveback();
delay(2000);
moveback();
}

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +3
    Very smooth movement, you are obviously making some good progress. Hopefully turning will be as smooth. Dubbie
  • DAB
    DAB over 7 years ago +3
    Good improvement over the original drive. DAB
  • genebren
    genebren over 7 years ago +2
    Great progress on your design challenge project. The platform is moving quite nicely. Keep up the good work! Gene
Parents
  • dubbie
    dubbie over 7 years ago

    Very smooth movement, you are obviously making some good progress. Hopefully turning will be as smooth.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago

    Very smooth movement, you are obviously making some good progress. Hopefully turning will be as smooth.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down