Sixth Sense Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sixth Sense Design Challenge
  • More
  • Cancel
Sixth Sense Design Challenge
Blog The Playground
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
  • Author Author: weiwei2
  • Date Created: 16 Dec 2018 3:06 AM Date Created
  • Views 1434 views
  • Likes 11 likes
  • Comments 4 comments
  • rover
  • robot
  • motor
Related
Recommended

The Playground

weiwei2
weiwei2
16 Dec 2018

Here is the venue of my weeding machine

image

it is a bit undulating, with different types of weeds and other stuff i don't want to cut (carpet grass, flower, other edible plant). Hence the idea is to 'sixth sense' those objects

Here let's take a look at all the objects

imageimage

i obviously cannot cut my children pet guinea pig, and the flowering plants that it like to devour.                     pumpkin and other flowering edible vegetation are not the target

 

and these are the target to cut

imageimage

a typical weed that i currently laboriously remove by hand                                                                                another variant of weed

image

these weed at the edge are a challenge, partly because they are taller, in addition there is a cement step border that might cause problem for my robot

 

Challenge

to build a robot that can traverse the garden with sixth sense (aka automated)

 

I am delighted that i am selected to be a contestant. The first thing is to find out all my existing rovers and see whether they can fit the bill. The first to try is whether they can move in the garden at all (i do know most of them should fail - image )

Here are them

imageimage

these are 4WD but the platform is too low and i guess they will easily get stuck

 

imageimage

the MiniQ can run the entire field but it is somewhat too fast and hard to maneuver as well                            Lego looks to be a possible candidate as the build can be customized, just that i need to interface with it special connector

  • Sign in to reply

Top Comments

  • weiwei2
    weiwei2 over 7 years ago +2
    actually, my surname is Leow, whereas my given name is Cheah Wei, so can call me Cheah Wei, or Leow I did some searching for past few days, on the chasis, and chance upon this. I am currently thinking…
  • jw0752
    jw0752 over 7 years ago +1
    Hi Cheah, This looks like it is going to be a fascinating challenge. You have laid out the challenge very well and I look forward to seeing how you conquer it. John
  • DAB
    DAB over 7 years ago +1
    Very cool project, I will be following your build with great interest. DAB
Parents
  • DAB
    DAB over 7 years ago

    Very cool project, I will be following your build with great interest.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 7 years ago

    Very cool project, I will be following your build with great interest.

     

    DAB