Smart Security and Surveillance
  • Challenges & Projects
  • Design Challenges
  • Smart Security and Surveillance
  • More
  • Cancel
Smart Security and Surveillance
Forum Sentinel Box - Part II - back to C
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Smart Security and Surveillance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 49 subscribers
  • Views 465 views
  • Users 0 members are here
  • security-challenge
  • rust
  • bmi160
  • MAX32630FTHR#
Related

Sentinel Box - Part II - back to C

saramic
saramic 6 months ago

I had fun with my Rust Crab experiment but it was time to get back to C  and LPSDK (Low Power ARM Micro SDK) if I was going to get anything complete for this challenge.

Recap

The idea is to build a smart lock box for digital devices to help control digital addiction, more on the idea can be found in part I

  • Sentinel Box - Part I - the plan

Rust for Hermetic builds

As I was not super happy in having to depend on EOL (End-of-life) software stacks like Mbed or LPSDK, I thought, how hard can it be writing a HAL (Hardware Abstraction Layer) from scratch in Rust. I had some initial wins getting the LED flashing, so I continued. In Part I I even started implementing some commands against the MAX14690 PMIC (Power Management Integrated Circuit) - I was actually going above and beyond and looking at the schematic of the dev board to see how it hangs together. This should have turned me OFF the idea of rust, but it gave me some false hope and I continued.

part of the MAX32630FTHR diagram highlighting the BMi160 accelerometer chip
The BMi160 accelerometer chip highlighted on the block diagram of the MAX32630FTHR

Next on the diagram there was an Accelerometer and Gyroscope using the BMi160 6-Axis Inertial Motion Sensor. With a bit of AI I soon enough had a driver to get X, Y, Z accelerations and using the MAX7219 I built a simple “attitude meter” which would show you which way to move the board to correct it being right way round. At this point I started to notice that some of the timing was out, my LED refresh rate was out by anywhere from 4x to 20x - that should have turned me OFF the idea of rust but with false hopes I continued.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The video above shows the attitude meter Airplane small️ that displays on the LED matrix the direction to turn the device to flatten the chip.

These were all distractions from the core of the Smart Security Challenge, so it was time to use a finger print reader. This would need UART (Universal Asynchronous Receiver-Transmitter) surely that cannot be hard? Well this is where the speed changes of 4X – 20X really started to bite. You see if you don’t know how fast your clock speed is going, you are not going to be able to transmit or receive at a given Baud. I tried a bunch of things. As I don’t have a logic analyzer nor oscilloscope on hand, I ended up hooking up an ESP32 to measure the duration of pulses. I didn’t know there was a function to measure pulse length pulseIn

unsigned long width = pulseIn(RX2_PIN, LOW, 5000000UL); // 5 s timeout
if (width == 0) {
  Serial.println("timeout — no signal on RX pin");
  return;
}
// Filter noise: allow 1200–115200 baud = 8–833 µs.
if (width < 8 || width > 833) {
  Serial.printf("noise/glitch: %lu µs (ignored)\n", width);
  return;
}
unsigned long estimated_baud = 1000000UL / width;
  // Square-wave formula: CPU MHz = N / width_µs, where N is the delay_cycles count.
  // Firmware step 1 uses N=4800. Steps double: 4800, 9600, 19200, 38400, 76800.
  // Read the first group of pulses (smallest width) and use N=4800.
Serial.printf(
  "LOW pulse: %lu µs | sq-wave asm::delay(4800)~9600 cycles: CPU ~%lu MHz\n",
  width,
  9600UL / width); // asm::delay(N) ≈ 2N cycles → CPU MHz = 9600 / width_µs

The above code also made me realise that \n does not cut it and my serial monitor only displayed the output when I had \r\n - need that Carriage return.

And all my Rust results were conclusive on 1 part, I was never getting 96 MHz. After some digging around I found the C file in LPSDK that seems to do the setup of the frequency

Maxim/Firmware/MAX3263X/Libraries/CMSIS/Device/Maxim/MAX3263X/Source/system_max3263x.c

  1. Enable the 32 kHz RTC oscillator — this serves as the stable reference clock for calibration, then wait for it to warm up and settle.
  2. Enable the RO calibration complete interrupt — so the system can signal when calibration is done.
  3. Clear the calibration complete interrupt flag — removing any stale state from a previous run.
  4. Write an initial trim value into the frequency calibration initial condition register — giving the hardware a starting point rather than hunting from scratch.
  5. Load that initial trim into the active frequency trim register — making it live.
  6. Enable the frequency control loop — the hardware mechanism that will drive the RO trim toward the target frequency.
  7. Start calibration in atomic mode — the hardware runs the measurement and adjustment cycle uninterrupted.
  8. Wait for the ro_cal_done flag — polling until the hardware signals completion.
  9. Stop the calibration engine.
  10. Disable the calibration complete interrupt.
  11. Read back the final trim value — the digital code the loop converged on.
  12. Write the final trim to the RO flash trim shadow register — persisting the result across resets.
  13. Restore the RTC to its previous state — since it may have been off before the routine borrowed it.
  14. Disable the frequency control loop.

no can do - I tried and tried again but could not get a consistent 96 MHz set which meant the UART was not going to work and the rust experiment was over for the time being

XCrab

Back to LPSDK

I couldn’t get myself to go to Mbed, a platform that is slated for EOL in July 2026, so it was back to C and the legacy LPSDK stack.

Hitting up my ESP32 setup, proved I had the right frequency set on UART and in no time I was connected to the fingerprint reader. The problem was that now my system would need to be multi modal. I pulled in a rotary encoder and got some runs on the board. First just to read turns to the left and right as well as a button press and display it on the LED MAX7219 matrix display. Then I added in the finger print reader.

Fingerprint reading success and failure

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Getting the fingerprint, LED Matrix and rotary encoder was the easy bit, but having a state diagram that can save a bunch of fingerprints and identify them was starting to get a bit complicated, as is the setup on my workbench.Encoder and fingerprint state machine flow chart

Next

Now that I have a basic fingerprint reader and a build system that I am confident in, I think I need to get the required piece for a minimal complete build, some kind of actuator working: stepper motor, servo motor or just a motor with a worm drive. This will allow me to create a lock box with multi finger print triggering. If I get time, I may be able to expand on that. Time will tell.

Source

https://github.com/saramic/sentinel-box

  • Sign in to reply
  • Cancel

Top Replies

  • arvindsa
    arvindsa 5 months ago +1
    Good to know i have a fellow developer in LPSDK
Parents
  • arvindsa
    arvindsa 5 months ago

    Good to know i have a fellow developer in LPSDK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • arvindsa
    arvindsa 5 months ago

    Good to know i have a fellow developer in LPSDK