Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 012
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 14 Nov 2013 12:39 PM Date Created
  • Views 757 views
  • Likes 0 likes
  • Comments 3 comments
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 012

COMPACT
COMPACT
14 Nov 2013

4 x 4 (Keypad that is!)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Yep, it's a 4 x 4 keypad. With a PSoC 4 you can make use of a 4 x 4 keypad without the need for creating any polling software.

With the inbuilt clocks and UDBs (Universal Digital Blocks) you can create a simple keypad scanner that presents a unique hexadecimal scan code for each key.

The scan code is a latched with an accompanying strobe signal to signify a key press to its consumer.

The schematic below includes additional NOT (aka inverter) gates to turn on the LEDs to represent '1' bits for the above video. These are normally excluded for normal use.

The hexadecimal scan code is made up of bits R_1, R_0, ED_0 and ED_1 in that order (MSB to LSB) for;

     0-3 Top row of keys from left to right

     4-7 2nd row of keys from left to right

     8-B 3rd row of keys from left to right

     C-F Bottom row of keys from left to right

image

 

Here is a picture of the Keypad row strobe generator output. Only one row is active at any time.

image

These are the ROW[3:0] signals. They are generated by Row address generator in combination with a LUT (Look Up Table).

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    Very cool demo, for the same reason as Gagan said..... This is like the patchboards we had in school, but than with a gazillion extra options and freedom!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago

    Very cool demo, for the same reason as Gagan said..... This is like the patchboards we had in school, but than with a gazillion extra options and freedom!