Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 014
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 16 Nov 2013 9:32 PM Date Created
  • Views 444 views
  • Likes 1 like
  • Comments 1 comment
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 014

COMPACT
COMPACT
16 Nov 2013

You've only got one shot at the title!

image

The Timer (2.5) component offers a two "One Shot" Run Mode configuration options.

  • One Shot
  • One Shot (Halt on Interrupt)

This article discusses the standard One Shot option.

"One Shot" means that the timer only runs one and then stops.

image

So with exactly the same basic default schematic but with a one shot option selected. The timer can run only once. As usual the timer is started with a Timer_Start() statement. The timer will start and when it reaches its TC (Terminal Count) it will stop.

For the above schematic diagram the LED will only change state once with no way to reset the and re-enable the timer because the its reset pin is connected to a logic '0'.

If you carefully read the component Timer's datasheet (Document Number: 001-86926 Rev. *A) at the bottom of page 24 is says;

 

     "After the One Shot period has completed, the Timer can be set up to run for another period by

     using a hardware reset. The hardware reset reloads the counter from the period register. One

     cycle after reset is removed, the Timer is enabled to count down again....."

 

I've found the easiest way to do this is to connect a digital input pin to the timer's reset pin.

This allows the timer to be reset by hardware or by software.

Ensure that this pin is usually kept low and only pulled high when you want to reset and re-enable the timer.

image

 

If you have any questions, please do not hesitate to leave a comment.

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    Good post.  It looks like you have several options to set up the timer to be more versatile with HW and SW control.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    Good post.  It looks like you have several options to set up the timer to be more versatile with HW and SW control.

     

    DAB