Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 022
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 28 Nov 2013 7:43 PM Date Created
  • Views 642 views
  • Likes 0 likes
  • Comments 1 comment
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 022

COMPACT
COMPACT
28 Nov 2013

The only good bug is a dead bug

image

 

Many Christmas Displays have animated figures.

I've put this test rig together to test out this project option. I've already demonstrated a PSoC 4 driving servo motors but servo motors are not always the desired option.

This time I've performed a quick test of getting an H bridge working with a PSoC 4.

 

I've used my PmodHB3. It contains an H-Bridge Driver for a single motor rated from 5-12V @ 2A.

I just used a plastic robot base and one of its toy motor connected to 3.3V which seemed to work

 

image

 

The schematic can't be simpler.

All it needs is two digital level output pins - Enable and Direction.

The Direction pin is used control them motor rotation direction which is either CW or CCW.

The Enable Pin is used to turn the motor on and off.

The Enable Pin can be pulse width modulated (PWM) to provide slower speeds (and subsequently lower torque output).

 

All an H-bridge really does is enable current to flow through a motor in either direction using four transistors under logic control.

Some circuits such as the PmodHB3 has some additional hardware logic gates to ensure that only valid combinations of the transistors are turned on.

The last thing one wants when using an H-bridge is to use the two wrong combinations as this creates an unwanted dead short circuit that bypasses the motor.


Unlike a servo motor there is no idea of the motor's current position.

If the motor's position is required then additional sensors are added.

 

image

The code to drive the motor couldn't be simpler either.

All that is required is to set the input pins to the desired state.

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    As you say, motor drive with the PSOC is a very simple program as long as you have the write hardware connected.

     

    A good H-bridge circuit is a easy as it gets.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Monte,

     

    As you say, motor drive with the PSOC is a very simple program as long as you have the write hardware connected.

     

    A good H-bridge circuit is a easy as it gets.

     

    DAB