Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog A Very Compact Christmas Display - Part 031
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 11 Dec 2013 11:43 AM Date Created
  • Views 733 views
  • Likes 0 likes
  • Comments 4 comments
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • psoc_4200
  • compact_xmas_display
  • smarter_life
  • psoc
Related
Recommended

A Very Compact Christmas Display - Part 031

COMPACT
COMPACT
11 Dec 2013

Processing Power

image

Here's the result of creating, importing and drawing the font for the LED display.

 

 

image

With the font captured in a 256 colour .BMP file for useable mspaint editing, I needed to import it into my program.

I've done this using Processing 2.1. If you haven't heard of Processing before have a look at the web http://processing.org.

I found it quite interesting and useful. According to its documentation it's actually not Java but Java based. Conversion from Processing to Java occurs when the Run button is clicked and that is what I observed.

I found it as easy to use as the Arduino and its derivatives considering the Arduino IDE was derived from Processing.

 

I always use symbolics for programming because it provides a very flexible and consistent means of reconfiguring software.

 

image

This code creates a comma delimited list with comments for direct use with source code. It can be very easily extended to insert indentation and data structure pre and post-amble to create a complete .h header file.

Code writing code?

 

image

 

I've inserted this generated code into my project and wrote a supporting drawletter() function to display the font on the LED display to display.

It's as easy to use as drawletter('A', x, y, colour);

  • Sign in to reply
Parents
  • bose
    bose over 12 years ago

    Hi,

     

    This is really good.

    Is it possible to share the source code for the Processing part?

    It would be really helpful.

     

    -Abhijit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 12 years ago in reply to bose

    The code presented in this article is Processing code.

    It only contains one function called setup().

    That's it.

    Very easy - Just remember that it is object oriented and requires the correct method for conversion between classes.

    e.g. from a character to a string using Character.tostring(cc)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • COMPACT
    COMPACT over 12 years ago in reply to bose

    The code presented in this article is Processing code.

    It only contains one function called setup().

    That's it.

    Very easy - Just remember that it is object oriented and requires the correct method for conversion between classes.

    e.g. from a character to a string using Character.tostring(cc)